1.3.1 Example Customer Key Encryption for SAMA5D3 Devices
secure-sam-ba-cipher.py customer-key -d sama5d3x -l license.txt -k cust.key -o
customer-key.cip90000
secure-sam-ba-cipher.py customer-key -d sama5d3x -l license.txt -k cust.key
-pad 0123456789abcdef -o customer-key.cip -pk license_private.pem -pp
pass:license_passphrase
Parameters:
-l, --license LICENSE (required)
Name of the file that contains the license.
-d, --device DEVICE (required)
Name of the device family.
-k, --key-file KEY_FILE (required)
Name of the file that contains the customer key.
-pad, --cust-key-padding KEY_PADDING (optional)
8-byte value used for customer key padding in hexadecimal format (only for SAMA5D3 devices). If omitted, random data will be used.
-o, --output-file OUTPUT_FILE (required)
Name of the file that will contain the ciphered customer key message.
-pk, --priv-key-file PRIVATE_KEY_FILE (required)
Name of the file that contains the license private key. This private key must be the one
generated by the request-license command.
-pp, --priv-key-pass PRIVATE_KEY_PASSWORD (optional)
Password used to decrypt the license private key. The syntax is
"pass:XXX" for password XXX, or "file:YYY" to read
password from file YYY. This parameter is mandatory if the license private key is
ciphered.