1.15 Low Power Modes
This example application shows how to enter Low Power modes of SAM9X75 MPU.
Description
The Clock system generates and distributes the clock for the processor and peripherals. This example application shows how device enters in the Idle mode and Ultra Low Power mode.
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/clock/low_power/firmware.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description |
|---|---|
| sam_9x75_curiosity.X | MPLABX project for SAM9X75 Curiosity Development Board |
| sam_9x75_curiosity_pro.X | MPLABX project for SAM9X75 Curiosity Pro Development Board |
Setting Up AT91Bootstrap Loader
To load the application binary onto the target device, the user needs to use at91bootstrap loader. Refer to the at91bootstrap loader documentation for details on how to configure, build and run bootstrap loader project and use it to bootstrap the application binaries.
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Description |
|---|---|
| sam_9x75_curiosity.X | SAM9X75 Curiosity Development Board |
| sam_9x75_curiosity_pro.X | SAM9X75 Curiosity Pro Development Board |
Setting Up SAM9X75 Curiosity Development Board
- Connect the UART DEBUG J35 on board to the computer using a UART-FTDI cable (to enable debug com port)
- Connect the USB port J2 on board to the computer using a micro USB cable (to power the board)
Setting Up SAM9X75 Curiosity Pro Development Board
- Connect the UART DEBUG J63 on board to the computer using a UART-FTDI cable (to enable debug com port)
- Connect the port J1 on board to the computer using a Type-C USB cable (to power the board)
Running the Application
- Build the application using its IDE.
- Open the Terminal application (Ex.:Tera term) on the computer.
- Connect to the (USB to Serial) COM port and configure the serial settings as
follows:
- Baud: 115200
- Data: 8 Bits
- Parity: None
- Stop: 1 Bit
- Flow Control: None
- LED toggles every 1 second.
- Press ‘0’ in the terminal
window:
- Observe the message “Entering Idle mode for 30 seconds” in the terminal window and LED stops toggling
- Wait for 30 seconds and observe the message “Leaving Idle mode” in the terminal window and LED toggles every 1 second
- Press ‘1’ in the terminal
window:
- Observe the message “Entering ULP0 mode for 30 seconds” in the terminal window and LED stops toggling
- Wait for 30 seconds and
observe the message “Leaving ULP0 mode” in the terminal window and LED
toggles every 1 second

| Board | LED Name |
|---|---|
| SAM9X75 Curiosity Development Board | RGB_LED (Blue) |
| SAM9X75 Curiosity Pro Development Board | RGB_LED (Blue) |