1 MPLAB® Harmony 3 Peripheral Library Application Examples for SAM9X7 Family
The following applications are provided to demonstrate the typical or interesting usage models of one or more peripheral libraries.
| Name | Description |
|---|---|
| ADC Automatic Window Comparison | This example application shows how to sample an analog input in Polled mode and send the converted data to console using automatic window comparison of converted values |
| ADC Low Power | This example application shows the different Low Power Sleep modes available with Fast Wake up either enabled or disabled |
| ADC Polling | This example application shows how to sample an analog input in Polled mode and send the converted data to console |
| Clock Configuration | This example application shows how to configure the clock system to run the device at maximum frequency. It outputs a prescaled clock signal on a GPIO pin for measurement and verification |
| DBGU Blocking | This example application demonstrates how to use the DBGU peripheral to transfer a block of data in a blocking manner |
| DBGU Interrupt | This example application demonstrates how to use the DBGU peripheral to transfer a block of data in a non-blocking manner |
| DBGU Ring Buffer | This example application shows how to use DBGU peripheral in Ring Buffer mode |
| FLEXCOM SPI EEPROM Read Write | This example application shows how to use the FLEXCOM module in SPI mode |
| FLEXCOM SPI Self Loopback DMA | This example application shows how to use the FLEXCOM SPI peripheral with DMA to transmit and receive a block of data |
| FLEXCOM TWI (I2C) EEPROM | This example application shows how to use the FLEXCOM module in TWI mode |
| FLEXCOM USART Flow Control | This example application shows how to use the FLEXCOM module in USART flow control mode |
| FLEXCOM ISO7816 SmartCard | This example application shows how to use the FLEXCOM module in ISO7816 SmartCard mode. |
| FLEXCOM LIN | This example application shows how to use the FLEXCOM module in LIN mode |
| FLEXCOM RS485 | This example application shows how to use the FLEXCOM module in RS485 mode |
| Low Power Modes | This example application shows how to enter Low Power modes of SAM9X75 MPU |
| MCAN FD Blocking | This example shows how to use the MCAN module to transmit and receive CAN FD messages in Polling mode |
| MCAN FD Interrupt | This example shows how to use the MCAN module to transmit and receive CAN FD messages in Interrupt mode |
| MCAN Interrupt | This example shows how to use the MCAN module to transmit and receive CAN messages in Interrupt mode |
| OTPC Read Write (Emulation) | This example application shows how to use the OTPC Peripheral library to perform OTP operations |
| PIO Interrupt | This example application shows how to generate GPIO interrupt on switch press and release, and indicate the switch status using the LED |
| PIO Polling | This example application shows how to poll the switch input, and indicate the switch status using the LED |
| PIT Period Change | This example application shows how PIT period can be changed during run time |
| PIT Polling | This example application shows how to use PIT counter in Polling mode |
| PIT Start Stop | This example application shows how PIT can be started and stopped at run time |
| PIT64B Periodic Interrupt | This application shows how to use PIT64B counter in Interrupt mode |
| PWM Channels | This example demonstrates how to use the PWM peripheral to generate PWM signals |
| QSPI Flash Read Write | This example application shows how to use the QSPI Peripheral library to perform erase, write and read operation with the QSPI Serial Flash memory in Quad IO mode |
| RSTC Interrupt | This example application shows how to use the RSTC peripheral to generate an interrupt instead of generating a reset, when the Reset switch is pressed on board |
| RSTC Reset Cause | This example shows how to use the RSTC peripheral to indicate the cause of the device reset |
| RTC Alarm Interrupt | This example application shows how to use the RTC to configure the time and generate the alarm |
| RTT Alarm Interrupt | This example application shows how to use the RTT to generate alarm interrupt |
| RTT Periodic Interrupt | This example application shows how to use the RTT to generate periodic interrupts |
| SHDWC Wakeup | This example application shows how to shutdown and wakeup the device using SHDWC peripheral |
| TC Capture Mode | This example application shows how to use the TC module in Capture mode to measure duty cycle and frequency of an external input |
| TC Compare Mode | This example application shows how to use the TC module in Compare mode to generate an active low, active high, and toggle output on compare match |
| TC Timer Mode | This example application shows how to use the TC module in Timer mode to generate periodic interrupt |
| TRNG Random Number | This example application shows how to use the TRNG Peripheral library to generate and read a random number |
| WDT Timeout | This example application shows how to generate a Watchdog timer reset by emulating a deadlock |
| XDMAC Memory Transfer | This example application shows how to use the XDMAC peripheral to do a memory to memory transfer and illustrates the usage of burst size to reduce the transfer time |