1.33 SHDWC Wakeup
This example application shows how to shutdown and wakeup the device using SHDWC peripheral.
Description
Application starts by toggling the LED, indicating that the device is up and running. Upon pressing the switch, it goes to Shutdown mode (stops toggling the LED). Upon pulling the START_PMIC pin to high, the device is reboot and the LED starts toggling again.
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/shdwc/shdwc_wakeup/firmware.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description |
|---|---|
| sam_9x75_curiosity.X | MPLABX project for SAM9X75 Curiosity Development Board |
| sam_9x75_curiosity_pro.X | MPLABX project for SAM9X75 Curiosity Pro Development Board |
Setting Up AT91Bootstrap Loader
To load the application binary onto the target device, the user needs to use at91bootstrap loader. Refer to the at91bootstrap loader documentation for details on how to configure, build and run bootstrap loader project and use it to bootstrap the application binaries.
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Description |
|---|---|
| sam_9x75_curiosity.X | SAM9X75 Curiosity Development Board |
| sam_9x75_curiosity_pro.X | SAM9X75 Curiosity Pro Development Board |
Setting Up SAM9X75 Curiosity Development Board
- SD card with FAT32 file system
- Download harmony MPU bootstrap loader from this location
- Copy the downloaded boot loader binary( boot.bin) onto the SD card
- SDMMC slot used for bootloading the application is SD BOOT (J14)
- Connect the UART DEBUG J35 on board to the computer using a UART-FTDI cable (to enable debug com port)
- Connect the USB port J2 on board to the computer using a micro USB cable (to power the board)
Setting Up SAM9X75 Curiosity Pro Development Board
- SD card with FAT32 file system
- Download harmony MPU bootstrap loader from this location
- Copy the downloaded boot loader binary( boot.bin) onto the SD card
- SDMMC slot used for bootloading the application is microSD (J42)
- Connect the UART DEBUG J63 on board to the computer using a UART-FTDI cable (to enable debug com port)
- Connect the port J1 on board to the computer using a Type-C USB cable (to power the board)
Running the Application
- Build the application using its IDE.
- Copy the output binary (named harmony.bin) onto the SD Card (Refer to the Setting up hardware section above for setting up the SD card).
- Insert the SD card into SDMMC slot on the board (Refer to the Setting up hardware section for the correct SDMMC slot).
- Reset the board to run the application.
- LED toggles indicating the board is up and running.
- Press Switch A to shutdown the device (LED toggling stops).
- Press Switch B to wakeup the device.
- Device resets (indicated by the LED starting to toggle again).
| Board | Switch A | Switch B | LED Name |
|---|---|---|---|
| SAM9X75 Curiosity Development Board | USER | START | RGB_LED (Blue) |
| SAM9X75 Curiosity Pro Development Board | USER | START | RGB_LED (Blue) |