5.1 Initialize the ADC
This subsection presents how to initialize the ADC module to run in the Free-Running Conversion mode. This application uses the Config A setup explained in Hardware Configuration. The FREERUN bit in ADC0.CTRLA must be set to activate this mode, in addition to the normal ADC initialization. When configuring the ADC in Free-Running mode, the next conversion starts immediately after the previous one.
This translates into the following code:
ADC0.CTRLA |= ADC_FREERUN_bm;
The ADC conversion is started by setting the STCONV bit in the ADC0.COMMAND register:
ADC0.COMMAND = ADC_STCONV_bm;
Then, the ADC results can be read in a while loop.