4.3 Get Code Examples from GitHub
The code examples are available through GitHub, which is a web-based server that provides
the application codes through a Graphical User Interface (GUI). The code examples can be
opened in both Microchip Studio and MPLAB X. To open the Microchip Studio project in
MPLAB X, select from the menu, ,
and navigate to the .cproj file.
The GitHub webpage: GitHub.
Code Examples
Finding code examples for devices in the tinyAVR 2 Family can be done by searching for the device name (e.g., ATtiny1627), in the GitHub example browser.
Download the code as a .zip file from the example page on
GitHub by clicking the Clone or download button.