14 Delay Driver
This Delay driver provides an interface for basic delay functions for applications requiring a brief wait during execution.
Summary of the API's Functional Features
Initialize the Delay driver and associated hardware
Delay for the given amount of microseconds
Delay for the given amount of milliseconds
Summary of Configuration Options
No configuration is needed in START.
Driver Implementation Description
The driver will first calculate the amount of cycles to delay for the given time according to the system clock, then use Systick to delay these cycles.
Example of Usage
The following shows a simple example of using the delay function. The delay driver must have been initialized by delay_init. This initialization will configure the operation of the SysTick.
void delay_example(void)
{
delay_ms(5000);
}
Dependencies
-
SysTick