10 STATUS FLAGS
- addrNotFound(0xFF/0xFFFF) – A read operation occurred on a previously unwritten data EEPROM address.
- expiredPage(0x1) – The program memory erase/write cycle count has exceeded the user-defined limit. The algorithm will attempt to execute the write operation.
- packBeforePageFull(0x2) – The pack routine was called before the currently active page was full. The routine will attempt to move the latest data EEPROM information to the packed page, even though the active page is not full.
- packBeforeInit(0x3) – The pack routine was executed before the initialization routine. The pack operation was aborted.
- packSkipped(0x4) – A page was written beyond the page boundary. This may be a result of the pack routine not being executed properly. The pack operation was aborted.
- illegalAddress(0x5) – There was an attempt to write/read with a data EEPROM address equal to or greater than the size of data EEPROM. The read/write operation was aborted.
- pageCorrupt(0x6) – The page status information was corrupted. The current operation was aborted.
- writeError(0x7) – The information that was written into program memory failed the verification. The current operation was aborted.
The status flags differ in severity and how they are serviced. The informational status flags are expected to occur during normal processing and are serviced by simply clearing the flag with the associated macro. These include: addrNotFound, packBeforePageFull and illegalAddress flags.
Warning status flags indicate a condition has been exceeded but processing will continue. This includes the expiredPage status flag. With this flag set, the algorithm will attempt to process read and write requests, but the flag will be set after each operation.
The most severe flags are the system error status flags. These imply either the integrity of the data EEPROM information has been compromised and/or the algorithm cannot continue until the offending condition has been resolved. These include packBeforeInit, pageCorrupt and writeError flags.
To avoid a packBeforeInit event, ensure the initialization routine, DEE_Init(), is called before performing any other emulation routine. Since this routine accesses the current state of the emulation process, it will take action only if it is required. Therefore, it can be called at any time during data EEPROM emulation.
The pageCorrupt and writeError flags indicate that a write operation failed to verify and the current operation was aborted. If this occurs, the integrity of the data EEPROM information has been compromised. No further emulation operations should be attempted. The memory reserved for data EEPROM emulation and attempt to reinitialize them.
Macros are available to retrieve and clear the status flag values. Status flags are cleared only by the user. No operation is affected by the value of any flag, but the flag’s value will indicate.