1.8 SpaceWire RMAP Loopback Example
This example shows how to configure the SpaceWire peripheral to configure the RMAP module, send an RMAP command with the packet transceiver and receive the RMAP reply with the packet receiver.
Building The Application
The parent folder for all the MPLABX IDE projects for this application is given below:
Application Path: aerospace\apps\spw\spw_rmap_loopback\firmware
To build the application, refer to the table below and open the appropriate project file in MPLABX IDE.
| Project Name | Description |
|---|---|
| sam_rh71_ek.X | SAM RH71 Evaluation Kit board |
MPLAB Harmony Configurations
Refer to the MCC project graph for the components used and the respective configuration options.
Hardware Setup
- Project sam_rh71_ek.X
- Hardware Used
- SAM RH71 Evaluation Kit
- SpaceWire cable
- Hardware Setup
- Connect the debugger probe to J33
- Connect the USB port on the board to the computer using a mini USB cable.
- Connect the two SpaceWire link on the board to each other using a SpaceWire cable.
- Hardware Used
Running The Application
Open the Terminal application (Ex.:Tera term) on the computer.
Connect to the Virtual COM port and configure the serial settings as follows:
- Baud : 115200
- Data : 8 Bits
- Parity : None
- Stop : 1 Bit
- Flow Control : None
Build and Program the application using the MPLABX IDE.
See the following message in the console.
----------------------------------------------------------- SPW RMAP loopback example ----------------------------------------------------------- Wait for both SWP link switch to run state SPW Link in Run state Initialize packet receiver to receive 1 packet(s) of 8 bytes Send SWP packet with RMAP command write with reply Wait RMAP reply Receive RMAP WRITE reply : ID = 0xabcd, with status : 0x0 RMAP write command reply with status OK Initialize packet receiver to receive 1 packet(s) of 80 bytes Send SWP packet with RMAP command read Wait RMAP reply Receive RMAP READ reply : ID = 0xabcd, with status : 0x0 Receive 64 bytes of data : 00, 01, 02, 03, 04, 05, 06, 07, 08, 09, 0A, 0B, 0C, 0D, 0E, 0F, 10, 11, 12, 13, 14, 15, 16, 17, 18, 19, 1A, 1B, 1C, 1D, 1E, 1F, 20, 21, 22, 23, 24, 25, 26, 27, 28, 29, 2A, 2B, 2C, 2D, 2E, 2F, 30, 31, 32, 33, 34, 35, 36, 37, 38, 39, 3A, 3B, 3C, 3D, 3E, 3F, RMAP read command reply with status OK