1.7 SpaceWire Loopback Example
This example shows how to configure the SpaceWire peripheral to send and receive multiple packets. It uses multiple receive buffer to exercise in an optimize way the 3 states (NEXT, CURRENT, PREVIOUS) for packet reception.
Building The Application
The parent folder for all the MPLABX IDE projects for this application is given below:
- Application Path : apps\spw\spw_loopback\firmware
To build the application, refer to the table below and open the appropriate project file in MPLABX IDE.
| Project Name | Description |
|---|---|
| sam_rh71_ek.X | SAM RH71 Evaluation Kit board |
MPLAB Harmony Configurations
Refer to the MCC project graph for the components used and the respective configuration options.
Hardware Setup
- Project sam_rh71_ek.X
- Hardware Used
- SAM RH71 Evaluation Kit
- SpaceWire cable
- Hardware Setup
- Connect the debugger probe to J33
- Connect the USB port on the board to the computer using a mini USB cable.
- Connect the two SpaceWire link on the board to each other using a SpaceWire cable.
- Hardware Used
Running The Application
Open the Terminal application (Ex.:Tera term) on the computer.
Connect to the Virtual COM port and configure the serial settings as follows:
- Baud : 115200
- Data : 8 Bits
- Parity : None
- Stop : 1 Bit
- Flow Control : None
Build and Program the application using the MPLABX IDE.
See the following message in the console.
----------------------------------------------------------- SPW loopback example ----------------------------------------------------------- Wait for both SWP link switch to run state SPW Link in Run state TX time=2284450 us, for 25000000 bytes Effective rate=87 Mb/s Average RX process time = 148 us Rx sequence errors = 0 End of transfer