7 How Oversampling Demo Application Works
In the example source code provided, ADC conversion is done in the functions
‘process_single_sampled()’ and
‘process_oversampled()’. For comparison, both oversampled and
normal ADC results are sent through USART to the serial terminal. Measured analog input
voltage (in volt) is displayed.
In the function ‘process_single_sampled()’, the ADC sample
accumulator has been configured to 1. The ADC result of only one sample is read. No
oversampling is done here.
The function ‘process_oversampled()’ demonstrates how the
oversampling is done and resolution has been increased from 10 to 12 bits. In the
function ‘process_oversampled()’, to get a 12-bit resolution from the
10-bit ADC it is required to read 16 ADC samples and then right shift the sum of the ADC
results by 2 (i.e. divide by 4).
To increase the resolution, for each additional bit of ADC resolution, n, the signal must be oversampled 4n. To achieve 12-bit ADC, you need an additional 2-bit resolution. Hence, the signal has to be sampled 42, i.e. 16 times more samples. The ADC has a configurable accumulator setting. This accumulator is configured to do 16 samples. The result in the ADC result register will then be the sum of the 16 samples. The scale factor, sf, is given by sf = 2n. The scale factor is the number the result may be divided by to scale the result to the desired bit width. In this example, the result is increased by two bits. Hence, the scale factor is 22 = 4. So the result may be divided by 4 or a right shift of 2 can be performed.
In both the ‘process_single_sampled()’ and
‘process_oversampled()’ functions, the ADC result is read and the
measured voltage has been converted to a string using the standard library function
‘dtostrf’ and this measured analog input voltage (in volt) has been
sent through USART to the serial terminal of the PC every 1 second.