7.5.4 Enum ac_chan_interrupt_selection
This enum is used to select when a channel interrupt should occur.
| Enum value | Description |
|---|---|
|
AC_CHAN_INTERRUPT_SELECTION_TOGGLE |
An interrupt will be generated when the comparator level is passed |
|
AC_CHAN_INTERRUPT_SELECTION_RISING |
An interrupt will be generated when the measurement goes above the compare level |
|
AC_CHAN_INTERRUPT_SELECTION_FALLING |
An interrupt will be generated when the measurement goes below the compare level |
|
AC_CHAN_INTERRUPT_SELECTION_END_OF_COMPARE |
An interrupt will be generated when a new measurement is complete. Interrupts will only be generated in single shot mode. This state needs to be cleared by the use of ac_chan_cleare_status() |