15.10 Interrupts
An interrupt is generated when the Flash controller clears the WR bit upon completion of a Flash program or erase operation. The interrupt event causes a CPU interrupt if it was configured and enabled in the NVIC. For the vector mapping table, see Nested Vector Interrupt Controller (NVIC) from Related Links. The interrupt occurs regardless of the outcome of the program or erase operation, successful or unsuccessful. The only exception is the No Operation (NOP) programming operation (NVMOP = 0), which is used to manually clear the error flags and does not create an interrupt event on completion but does clear the WR bit.
The Flash Controller interrupts are not persistent, and, therefore, there is no need for an additional step to clear the cause or source of the interrupt.
After configuring the interrupt controller, the Flash event causes the CPU to jump to the vector assigned to the Flash event. The CPU starts executing the code at the vector address. The user software at this vector address must perform the required operations and, then, exit.