2.3 CBG Driver
Overview
The Current Bias Generator (CBG) consists of two classes of current sources: 10 µA and 50 µA sources.
-
10 µA Current Sources
- Current sourcing only.
- Up to four independent sources.
-
50 µA Current Sources
- Selectable current sourcing or sinking.
- Selectable current mirroring for sourcing and sinking.
Features
- Simultaneous generation of 10uA and 50uA current source or sink on dedicated output pins.
- Enabling 10uA current sources and 50uA current source or sink enables the corresponding output pin as well.
- Current mirror mode is supported only in 50uA source.
2.3.1 Module Documentation
2.3.1.1 CBG Driver
Current Bias Generator driver is to configure 10uA and 50uA current sources using dsPIC MCUs.
2.3.1.1.1 Module description
Current Bias Generator driver is to configure 10uA and 50uA current sources using dsPIC MCUs.
Data structures
struct CBG_INTERFACE
Structure containing the function pointers of CBG driver.
Functions
void CBG_Initialize (void)
Initializes CBG module.
void CBG_Deinitialize (void)
Deinitializes the CBG to POR values.
static void CBG_Enable (void)
This inline function enables the CBG module.
static void CBG_Disable (void)
This inline function disables the CBG module.
Variables
const struct CBG_INTERFACE CBG
Structure object of type CBG_INTERFACE with the custom name given by the user in the Melody Driver User interface.
2.3.1.1.2 Function Documentation
CBG_Deinitialize()
void CBG_Deinitialize (void )
Deinitializes the CBG to POR values.
| none |
none |
CBG_Disable()
inline static void CBG_Disable (void )
This inline function disables the CBG module.
The CBG_Initialize function should be called before calling this function. |
| none |
none |
CBG_Enable()
inline static void CBG_Enable (void )
This inline function enables the CBG module.
The CBG_Initialize function should be called before calling this function. |
none |
CBG_Initialize()
void CBG_Initialize (void )
Initializes CBG module.
| none |
none |
2.3.1.1.3 Variable Documentation
CBG
const struct CBG_INTERFACE CBG
Structure object of type CBG_INTERFACE with the custom name given by the user in the Melody Driver User interface.
The default name e.g. CBG can be changed by the user in the CBG user interface. This allows defining a structure with application specific name using the 'Custom Name' field. Application specific name allows the API Portability.
2.3.2 Class Documentation
2.3.2.1 CBG_INTERFACE Struct Reference
Structure containing the function pointers of CBG driver.
2.3.2.1.1 Detailed Description
Structure containing the function pointers of CBG driver.
#include <cbg_interface.h>
Public Attributes
void(* Initialize )(void)
Pointer to CBG_Initialize.
void(* Deinitialize )(void)
Pointer to CBG_Deinitialize.
void(* Enable )(void)
Pointer to CBG_Enable.
void(* Disable )(void)
Pointer to CBG_Disable.
2.3.2.1.2 Member Data Documentation
Deinitialize
void(* Deinitialize) (void)
Pointer to CBG_Deinitialize.
Disable
void(* Disable) (void)
Pointer to CBG_Disable.
Enable
void(* Enable) (void)
Pointer to CBG_Enable.
Initialize
void(* Initialize) (void)
Pointer to CBG_Initialize.
2.3.3 File Documentation
2.3.3.1 source/cbg.h File Reference
This is the generated driver header file for the CBG driver.
#include <xc.h> #include "cbg_interface.h"
2.3.3.1.1 Functions
void CBG_Initialize (void)
Initializes CBG module.
void CBG_Deinitialize (void)
Deinitializes the CBG to POR values.
static void CBG_Enable (void)
This inline function enables the CBG module.
static void CBG_Disable (void)
This inline function disables the CBG module.
2.3.3.1.2 Variables
const struct CBG_INTERFACE CBG
Structure object of type CBG_INTERFACE with the custom name given by the user in the Melody Driver User interface.
2.3.3.1.3 Detailed Description
This is the generated driver header file for the CBG driver.
CBG Generated Driver Header File
2.3.3.2 source/cbg_interface.h File Reference
2.3.3.2.1 Data structures
struct CBG_INTERFACE
Structure containing the function pointers of CBG driver.
2.3.3.2.2 Detailed Description
CBG Generated Driver Interface Header File