2.9 Event Output Driver
Overview
Event output is the change in the state of the pin output to high or low or to toggle after a specific time interval.Event output is the change in the state of the pin output to high or low or to toggle after a specific time interval.
Features
- User configurable event change type, i,e to set the event output pin high or low, to toggle when the transition time elapses.
- Event Transition time is user configurable, this value range varies based on the clock source selected from Hardware Dependency module (PLIB).
- In Synchronization (Sync) operation, the timer Reset or clear occurs when the input selected by Sync is asserted.
- In Trigger operation, the Timer is held in Reset until the input selected by Trigger is asserted.
The following waveform represents the Event Output generation and the effect of Sync signal assertion.The following waveform represents the Event Output generation and the effect of Sync signal assertion.
The following waveform represents the Trigger source effect on Event Output generation The following waveform represents the Trigger source effect on Event Output generation
2.9.1 Module Documentation
2.9.1.1 Event Output Driver
Event output Driver is used to generate single or series of Low, High or Toggle Output using dsPIC MCUs.
2.9.1.1.1 Module description
Event output Driver is used to generate single or series of Low, High or Toggle Output using dsPIC MCUs.
Data structures
struct EVENTOUTPUT_INTERFACE
Structure containing the function pointers of EVENTOUTPUT driver.
Definitions
#define Event_Output9_Initialize MCCP9_EventOutput_Initialize
This macro defines the Custom Name for MCCP9_EventOutput_Initialize API.
#define Event_Output9_Deinitialize MCCP9_EventOutput_Deinitialize
This macro defines the Custom Name for MCCP9_EventOutput_Deinitialize API.
#define Event_Output9_Enable MCCP9_EventOutput_Enable
This macro defines the Custom Name for MCCP9_EventOutput_Enable API.
#define Event_Output9_Disable MCCP9_EventOutput_Disable
This macro defines the Custom Name for MCCP9_EventOutput_Disable API.
#define Event_Output9_TransitTimeSet MCCP9_EventOutput_TransitTimeSet
This macro defines the Custom Name for MCCP9_EventOutput_TransitTimeSet API.
#define Event_Output9_SoftwareTriggerSet MCCP9_EventOutput_SoftwareTriggerSet
This macro defines the Custom Name for MCCP9_EventOutput_SoftwareTriggerSet API.
#define Event_Output9_Tasks MCCP9_EventOutput_Tasks
This macro defines the Custom Name for MCCP9_EventOutput_Tasks API.
#define Event_Output9_EventOutput_CallbackRegister MCCP9_EventOutput_CallbackRegister
This macro defines the Custom Name for MCCP9_EventOutput_CallbackRegister API.
Functions
void MCCP9_EventOutput_Initialize (void)
Initializes the MCCP9 Edge Event driver. This function must be called before any other MCCP9 function is called.
void MCCP9_EventOutput_Deinitialize (void)
Deinitializes the MCCP9 to POR values.
void MCCP9_EventOutput_Enable (void)
Enables the MCCP9 module with the corresponding operation mode.
void MCCP9_EventOutput_Disable (void)
Disables the MCCP9 module.
void MCCP9_EventOutput_TransitTimeSet (size_t count)
Sets the compare values for MCCP9.
void MCCP9_EventOutput_SoftwareTriggerSet (void)
Sets the software trigger.
void MCCP9_EventOutput_CallbackRegister (void(*handler)(void))
This function can be used to override default callback and to define custom callback for MCCP9 EventOutput event.
void MCCP9_EventOutput_Callback (void)
This is the default callback with weak attribute. The user can override and implement the default callback without weak attribute or can register a custom callback function using MCCP9_EventOutput_CallbackRegister.
void MCCP9_EventOutput_Tasks (void)
This function is used to implement the tasks for polled implementations.
Variables
const struct EVENTOUTPUT_INTERFACE Event_Output9
Structure object of type EVENTOUTPUT_INTERFACE with the custom name given by the user in the Melody Driver User interface.
2.9.1.1.2 Definition Documentation
Event_Output9_Deinitialize
#define Event_Output9_Deinitialize MCCP9_EventOutput_Deinitialize
This macro defines the Custom Name for MCCP9_EventOutput_Deinitialize API.
Event_Output9_Disable
#define Event_Output9_Disable MCCP9_EventOutput_Disable
This macro defines the Custom Name for MCCP9_EventOutput_Disable API.
Event_Output9_Enable
#define Event_Output9_Enable MCCP9_EventOutput_Enable
This macro defines the Custom Name for MCCP9_EventOutput_Enable API.
Event_Output9_EventOutput_CallbackRegister
#define Event_Output9_EventOutput_CallbackRegister MCCP9_EventOutput_CallbackRegister
This macro defines the Custom Name for MCCP9_EventOutput_CallbackRegister API.
Event_Output9_Initialize
#define Event_Output9_Initialize MCCP9_EventOutput_Initialize
This macro defines the Custom Name for MCCP9_EventOutput_Initialize API.
Event_Output9_SoftwareTriggerSet
#define Event_Output9_SoftwareTriggerSet MCCP9_EventOutput_SoftwareTriggerSet
This macro defines the Custom Name for MCCP9_EventOutput_SoftwareTriggerSet API.
Event_Output9_Tasks
#define Event_Output9_Tasks MCCP9_EventOutput_Tasks
This macro defines the Custom Name for MCCP9_EventOutput_Tasks API.
Event_Output9_TransitTimeSet
#define Event_Output9_TransitTimeSet MCCP9_EventOutput_TransitTimeSet
This macro defines the Custom Name for MCCP9_EventOutput_TransitTimeSet API.
2.9.1.1.3 Function Documentation
MCCP9_EventOutput_Callback()
void MCCP9_EventOutput_Callback (void )
This is the default callback with weak attribute. The user can override and implement the default callback without weak attribute or can register a custom callback function using MCCP9_EventOutput_CallbackRegister.
| none |
none |
MCCP9_EventOutput_CallbackRegister()
void MCCP9_EventOutput_CallbackRegister (void(*)(void) handler)
This function can be used to override default callback and to define custom callback for MCCP9 EventOutput event.
| in | handler |
- Address of the callback function |
none |
MCCP9_EventOutput_Deinitialize()
void MCCP9_EventOutput_Deinitialize (void )
Deinitializes the MCCP9 to POR values.
| none |
none |
MCCP9_EventOutput_Disable()
void MCCP9_EventOutput_Disable (void )
Disables the MCCP9 module.
| none |
none |
MCCP9_EventOutput_Enable()
void MCCP9_EventOutput_Enable (void )
Enables the MCCP9 module with the corresponding operation mode.
| none |
none |
MCCP9_EventOutput_Initialize()
void MCCP9_EventOutput_Initialize (void )
Initializes the MCCP9 Edge Event driver. This function must be called before any other MCCP9 function is called.
| none |
none |
MCCP9_EventOutput_SoftwareTriggerSet()
void MCCP9_EventOutput_SoftwareTriggerSet (void )
Sets the software trigger.
| none |
none |
MCCP9_EventOutput_Tasks()
void MCCP9_EventOutput_Tasks (void )
This function is used to implement the tasks for polled implementations.
| none |
none |
MCCP9_EventOutput_TransitTimeSet()
void MCCP9_EventOutput_TransitTimeSet (size_t count)
Sets the compare values for MCCP9.
| in | count |
- edge event wait time count |
none |
2.9.1.1.4 Variable Documentation
Event_Output9
const struct EVENTOUTPUT_INTERFACE Event_Output9
Structure object of type EVENTOUTPUT_INTERFACE with the custom name given by the user in the Melody Driver User interface.
The default name e.g. Event_Output1 can be changed by the user in the MCCP user interface. This allows defining a structure with application specific name using the 'Custom Name' field. Application specific name allows the API Portability.
2.9.2 Class Documentation
2.9.2.1 EVENTOUTPUT_INTERFACE Struct Reference
Structure containing the function pointers of EVENTOUTPUT driver.
2.9.2.1.1 Detailed Description
Structure containing the function pointers of EVENTOUTPUT driver.
#include <eventoutput_interface.h>
Public Attributes
void(* Initialize )(void)
Pointer to SCCPx_EventOutput_Initialize e.g. SCCP1_EventOutput_Initialize.
void(* Deinitialize )(void)
Pointer to SCCPx_EventOutput_Deinitialize e.g. SCCP1_EventOutput_Deinitialize.
void(* Enable )(void)
Pointer to SCCPx_EventOutput_Enable e.g. SCCP1_EventOutput_Enable.
void(* Disable )(void)
Pointer to SCCPx_EventOutput_Disable e.g. SCCP1_EventOutput_Disable.
void(* TransitTimeSet )(size_t count)
Pointer to SCCPx_EventOutput_TransitTimeSet e.g. SCCP1_EventOutput_TransitTimeSet.
void(* SoftwareTriggerSet )(void)
Pointer to SCCPx_EventOutput_SoftwareTriggerSet e.g. SCCP1_EventOutput_SoftwareTriggerSet.
void(* CallbackRegister )(void(*handler)(void))
Pointer to SCCPx_EventOutput_CallbackRegister e.g. SCCP1_EventOutput_CallbackRegister.
void(* Tasks )(void)
Pointer to SCCPx_EventOutput_Tasks e.g. SCCP1_EventOutput_Tasks (Supported only in polling mode)
2.9.2.1.2 Member Data Documentation
The documentation for this struct was generated from the following file:
source/
CallbackRegister
void(* CallbackRegister) (void(*handler)(void))
Pointer to SCCPx_EventOutput_CallbackRegister e.g. SCCP1_EventOutput_CallbackRegister.
Deinitialize
void(* Deinitialize) (void)
Pointer to SCCPx_EventOutput_Deinitialize e.g. SCCP1_EventOutput_Deinitialize.
Disable
void(* Disable) (void)
Pointer to SCCPx_EventOutput_Disable e.g. SCCP1_EventOutput_Disable.
Enable
void(* Enable) (void)
Pointer to SCCPx_EventOutput_Enable e.g. SCCP1_EventOutput_Enable.
Initialize
void(* Initialize) (void)
Pointer to SCCPx_EventOutput_Initialize e.g. SCCP1_EventOutput_Initialize.
SoftwareTriggerSet
void(* SoftwareTriggerSet) (void)
Pointer to SCCPx_EventOutput_SoftwareTriggerSet e.g. SCCP1_EventOutput_SoftwareTriggerSet.
Tasks
void(* Tasks) (void)
Pointer to SCCPx_EventOutput_Tasks e.g. SCCP1_EventOutput_Tasks (Supported only in polling mode)
TransitTimeSet
void(* TransitTimeSet) (size_t count)
Pointer to SCCPx_EventOutput_TransitTimeSet e.g. SCCP1_EventOutput_TransitTimeSet.
2.9.3 File Documentation
2.9.3.1 source/eventoutput_interface.h File Reference
#include <stddef.h>
2.9.3.1.1 Data structures
struct EVENTOUTPUT_INTERFACE
Structure containing the function pointers of EVENTOUTPUT driver.
2.9.3.1.2 Detailed Description
EVENTOUTPUT Generated Driver Interface Header File
2.9.3.2 source/mccp9.h File Reference
This is the generated driver header file for the MCCP9 driver.
#include <stddef.h> #include "eventoutput_interface.h"
2.9.3.2.1 Functions
void MCCP9_EventOutput_Initialize (void)
Initializes the MCCP9 Edge Event driver. This function must be called before any other MCCP9 function is called.
void MCCP9_EventOutput_Deinitialize (void)
Deinitializes the MCCP9 to POR values.
void MCCP9_EventOutput_Enable (void)
Enables the MCCP9 module with the corresponding operation mode.
void MCCP9_EventOutput_Disable (void)
Disables the MCCP9 module.
void MCCP9_EventOutput_TransitTimeSet (size_t count)
Sets the compare values for MCCP9.
void MCCP9_EventOutput_SoftwareTriggerSet (void)
Sets the software trigger.
void MCCP9_EventOutput_CallbackRegister (void(*handler)(void))
This function can be used to override default callback and to define custom callback for MCCP9 EventOutput event.
void MCCP9_EventOutput_Callback (void)
This is the default callback with weak attribute. The user can override and implement the default callback without weak attribute or can register a custom callback function using MCCP9_EventOutput_CallbackRegister.
void MCCP9_EventOutput_Tasks (void)
This function is used to implement the tasks for polled implementations.
2.9.3.2.2 Macros
#define Event_Output9_Initialize MCCP9_EventOutput_Initialize
This macro defines the Custom Name for MCCP9_EventOutput_Initialize API.
#define Event_Output9_Deinitialize MCCP9_EventOutput_Deinitialize
This macro defines the Custom Name for MCCP9_EventOutput_Deinitialize API.
#define Event_Output9_Enable MCCP9_EventOutput_Enable
This macro defines the Custom Name for MCCP9_EventOutput_Enable API.
#define Event_Output9_Disable MCCP9_EventOutput_Disable
This macro defines the Custom Name for MCCP9_EventOutput_Disable API.
#define Event_Output9_TransitTimeSet MCCP9_EventOutput_TransitTimeSet
This macro defines the Custom Name for MCCP9_EventOutput_TransitTimeSet API.
#define Event_Output9_SoftwareTriggerSet MCCP9_EventOutput_SoftwareTriggerSet
This macro defines the Custom Name for MCCP9_EventOutput_SoftwareTriggerSet API.
#define Event_Output9_Tasks MCCP9_EventOutput_Tasks
This macro defines the Custom Name for MCCP9_EventOutput_Tasks API.
#define Event_Output9_EventOutput_CallbackRegister MCCP9_EventOutput_CallbackRegister
This macro defines the Custom Name for MCCP9_EventOutput_CallbackRegister API.
2.9.3.2.3 Variables
const struct EVENTOUTPUT_INTERFACE Event_Output9
Structure object of type EVENTOUTPUT_INTERFACE with the custom name given by the user in the Melody Driver User interface.
2.9.3.2.4 Detailed Description
This is the generated driver header file for the MCCP9 driver.
MCCP9 Generated Driver Header File