2.25 SPI Client Driver
2.25.1 Introduction
Overview
The Serial Peripheral Interface (SPI) module is a synchronous serial interface useful for communicating with other peripheral or microcontroller devices. These peripheral devices can be serial EEPROMs, Shift registers, display drivers, Analog-to-Digital Converters and so on.
Features
- Allows to setup multiple Client Configurations to interact with multiple hosts having different configurations. SPIx_Open and SPIx_Close are the APIs to be used for selecting/switching between different Client configurations at run time.
- SPI Mode is configurable for each Client Configuration table entry.
- User can provide Custom Name for each Client Configuration table entry.
- Supports Enhanced Buffer mode with communication width of 8 bit only.
- Currently, only polling mode is supported.
2.25.2 Module Documentation
2.25.2.1 SPI Client Driver
Serial Peripheral Interface (SPI) CLIENT Driver using dsPIC MCUs.
2.25.2.1.1 Module description
Serial Peripheral Interface (SPI) CLIENT Driver using dsPIC MCUs.
2.25.2.1.1.1 Data structures
struct SPI_CLIENT_INTERFACE
Structure containing the function pointers of SPI CLIENT driver.
2.25.2.1.1.2 Enumerations
enum SPI1_CLIENT_USER_CONFIG { CLIENT_CONFIG }
Enum list is the Custom names for the SPI1 CLIENT multiple configuration, configured by user in MCC Melody user interface.
2.25.2.1.1.3 Functions
void SPI1_Initialize (void)
Initializes SPI1 module, using the given initialization data. This function must be called before any other SPI1 function is called.
void SPI1_Deinitialize (void)
Deinitializes the SPI1 to POR values.
void SPI1_Close (void)
Disables the SPI1 module.
bool SPI1_Open (uint8_t spiConfigIndex)
Configures SPI1 module with user defined unique configuration.
uint8_t SPI1_ByteExchange (uint8_t byteData)
Exchanges one byte of data. This is a blocking function.
void SPI1_ByteWrite (uint8_t byteData)
Writes one byte of data.
uint8_t SPI1_ByteRead (void)
Reads one byte of data from SPI1.
bool SPI1_IsRxReady (void)
Returns a boolean value if data is available to read.
bool SPI1_IsTxReady (void)
Returns a boolean value if data can be written.
2.25.2.1.1.4 Variables
const struct SPI_CLIENT_INTERFACE SPI1_Client
Structure object of type SPI_CLIENT_INTERFACE assigned with name displayed in the Melody Driver User interface. A structure pointer can be used to achieve portability across the SPI CLIENT having same interface structure.
2.25.2.1.2 Function Documentation
2.25.2.1.2.1 SPI1_ByteExchange()
uint8_t SPI1_ByteExchange (uint8_t byteData)
Exchanges one byte of data. This is a blocking function.
The SPI1_IsTxReady function must be called before calling this function. |
| in | data- |
Data byte to be exchanged. |
none |
2.25.2.1.2.2 SPI1_ByteRead()
uint8_t SPI1_ByteRead (void )
Reads one byte of data from SPI1.
The SPI1_IsRxReady function must be called before calling this function. Also note that byte read must be after byte write sequence. |
| none |
Data read from SPI1. |
2.25.2.1.2.3 SPI1_ByteWrite()
void SPI1_ByteWrite (uint8_t byteData)
Writes one byte of data.
The SPI1_IsTxReady function must be called before calling this function. Also note that every byte write has to be followed by a byte read. |
| in | byteData |
- Data to be written. |
none |
2.25.2.1.2.4 SPI1_Close()
void SPI1_Close (void )
Disables the SPI1 module.
The SPI1_Open function must be called before calling this function. |
| none |
none |
2.25.2.1.2.5 SPI1_Deinitialize()
void SPI1_Deinitialize (void )
Deinitializes the SPI1 to POR values.
| none |
none |
2.25.2.1.2.6 SPI1_Initialize()
void SPI1_Initialize (void )
Initializes SPI1 module, using the given initialization data. This function must be called before any other SPI1 function is called.
| none |
none |
2.25.2.1.2.7 SPI1_IsRxReady()
bool SPI1_IsRxReady (void )
Returns a boolean value if data is available to read.
The SPI1_Open function must be called before calling this function. |
| none |
true - Data available to read false - Data not available to read |
2.25.2.1.2.8 SPI1_IsTxReady()
bool SPI1_IsTxReady (void )
Returns a boolean value if data can be written.
The SPI1_Open function must be called before calling this function. |
| none |
true - Data can be written false - Data buffer is full |
2.25.2.1.2.9 SPI1_Open()
bool SPI1_Open (uint8_t spiConfigIndex)
Configures SPI1 module with user defined unique configuration.
| in | spiConfigIndex |
- SPI1_USER_CONFIG Enum value |
| none |
bool true - SPI1 is configured successfully. bool false - SPI1 is not configured successfully. |
2.25.2.1.3 Enumeration Type Documentation
2.25.2.1.3.1 SPI1_CLIENT_USER_CONFIG
enum SPI1_CLIENT_USER_CONFIG
Enum list is the Custom names for the SPI1 CLIENT multiple configuration, configured by user in MCC Melody user interface.
The enum list in the Help document might be just a reference to illustrate multiple configuration. Generated enum list is based on the configuration done by user in the MCC Melody user interface
| CLIENT_CONFIG |
Custom name for configuration setting: SPI Mode : Mode 1 |
2.25.2.1.4 Variable Documentation
2.25.2.1.4.1 SPI1_Client
const struct SPI_CLIENT_INTERFACE SPI1_Client
Structure object of type SPI_CLIENT_INTERFACE assigned with name displayed in the Melody Driver User interface. A structure pointer can be used to achieve portability across the SPI CLIENT having same interface structure.
2.25.3 Class Documentation
2.25.3.1 SPI_CLIENT_INTERFACE Struct Reference
Structure containing the function pointers of SPI CLIENT driver.
2.25.3.1.1 Detailed Description
Structure containing the function pointers of SPI CLIENT driver.
#include <spi_client_interface.h>
2.25.3.1.1.1 Public Attributes
void(* Initialize )(void)
Pointer to SPIx_Initialize e.g. SPI1_Initialize.
void(* Deinitialize )(void)
Pointer to SPIx_Deinitialize e.g. SPI1_Deinitialize.
void(* Close )(void)
Pointer to SPIx_Close e.g. SPI1_Close.
bool(* Open )(uint8_t spiConfigIndex)
Pointer to SPIx_Open e.g. SPI1_Open.
uint8_t(* ByteExchange )(uint8_t byteData)
Pointer to SPIx_ByteExchange e.g. SPI1_ByteExchange.
uint8_t(* ByteRead )(void)
Pointer to SPIx_ByteRead e.g. SPI1_ByteRead.
void(* ByteWrite )(uint8_t byteData)
Pointer to SPIx_ByteWrite e.g. SPI1_ByteWrite.
bool(* IsRxReady )(void)
Pointer to SPIx_IsRxReady e.g. SPI1_IsRxReady.
bool(* IsTxReady )(void)
Pointer to SPIx_IsTxReady e.g. SPI1_IsTxReady.
2.25.3.1.2 Member Data Documentation
The documentation for this struct was generated from the following file:
source/
2.25.3.1.2.1 ByteExchange
uint8_t(* ByteExchange) (uint8_t byteData)
Pointer to SPIx_ByteExchange e.g. SPI1_ByteExchange.
2.25.3.1.2.2 ByteRead
uint8_t(* ByteRead) (void)
Pointer to SPIx_ByteRead e.g. SPI1_ByteRead.
2.25.3.1.2.3 ByteWrite
void(* ByteWrite) (uint8_t byteData)
Pointer to SPIx_ByteWrite e.g. SPI1_ByteWrite.
2.25.3.1.2.4 Close
void(* Close) (void)
Pointer to SPIx_Close e.g. SPI1_Close.
2.25.3.1.2.5 Deinitialize
void(* Deinitialize) (void)
Pointer to SPIx_Deinitialize e.g. SPI1_Deinitialize.
2.25.3.1.2.6 Initialize
void(* Initialize) (void)
Pointer to SPIx_Initialize e.g. SPI1_Initialize.
2.25.3.1.2.7 IsRxReady
bool(* IsRxReady) (void)
Pointer to SPIx_IsRxReady e.g. SPI1_IsRxReady.
2.25.3.1.2.8 IsTxReady
bool(* IsTxReady) (void)
Pointer to SPIx_IsTxReady e.g. SPI1_IsTxReady.
2.25.3.1.2.9 Open
bool(* Open) (uint8_t spiConfigIndex)
Pointer to SPIx_Open e.g. SPI1_Open.
2.25.4 File Documentation
2.25.4.1 source/spi1.h File Reference
This is the generated driver header file for the SPI1 driver.
#include <stdint.h> #include <stdbool.h> #include <stddef.h> #include "spi_client_interface.h"
2.25.4.1.1 Functions
void SPI1_Initialize (void)
Initializes SPI1 module, using the given initialization data. This function must be called before any other SPI1 function is called.
void SPI1_Deinitialize (void)
Deinitializes the SPI1 to POR values.
void SPI1_Close (void)
Disables the SPI1 module.
bool SPI1_Open (uint8_t spiConfigIndex)
Configures SPI1 module with user defined unique configuration.
uint8_t SPI1_ByteExchange (uint8_t byteData)
Exchanges one byte of data. This is a blocking function.
void SPI1_ByteWrite (uint8_t byteData)
Writes one byte of data.
uint8_t SPI1_ByteRead (void)
Reads one byte of data from SPI1.
bool SPI1_IsRxReady (void)
Returns a boolean value if data is available to read.
bool SPI1_IsTxReady (void)
Returns a boolean value if data can be written.
2.25.4.1.2 Enumerations
enum SPI1_CLIENT_USER_CONFIG { CLIENT_CONFIG }
Enum list is the Custom names for the SPI1 CLIENT multiple configuration, configured by user in MCC Melody user interface.
2.25.4.1.3 Variables
const struct SPI_CLIENT_INTERFACE SPI1_Client
Structure object of type SPI_CLIENT_INTERFACE assigned with name displayed in the Melody Driver User interface. A structure pointer can be used to achieve portability across the SPI CLIENT having same interface structure.
2.25.4.1.4 Detailed Description
This is the generated driver header file for the SPI1 driver.
SPI1 Generated Driver Header File
2.25.4.2 source/spi_client_interface.h File Reference
#include <stdint.h> #include <stdbool.h> #include <stddef.h>
2.25.4.2.1 Data structures
struct SPI_CLIENT_INTERFACE
Structure containing the function pointers of SPI CLIENT driver.
2.25.4.2.2 Detailed Description
SPI Generated Driver Interface Header File