5.3.3 Approved Antenna Types
To maintain modular approval in the United States, only the antenna types that have been tested shall be used. Antennas approved for A09-3167 with the antenna types are listed in Table 5-1.
Antenna Requirement: 47CFR section 15.203
CAUTION: This equipment must be professionally installed. The installer shall be
responsible for ensuring that only the supplied antenna is employed so that the limits
in this part are not exceeded. Nonprofessional installation or installation of the
equipment with an improper antenna may void the equipment authorization from the FCC and
will void the Microchip warranty.