1 Harmony 3 Driver, System Services and RTOS Application Examples for PIC32CX MT Family
MPLAB® Harmony 3 is an extension of the MPLAB® ecosystem for creating embedded firmware solutions for Microchip 32-bit SAM and PIC® microcontroller and microprocessor devices. Refer to the following links for more information.
- Microchip 32-bit MCUs
- Microchip 32-bit MPUs
- Microchip MPLAB X IDE
- Microchip MPLAB® Harmony
- Microchip MPLAB® Harmony Pages
This repository contains the MPLAB® Harmony 3 driver and system service application examples for PIC32CX MT family:
To clone or download these applications from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Contents Summary
Folder | Description |
---|---|
apps | Contains driver and system service example applications |
Code Examples
Name | Description |
---|---|
1.1 Console Debug System Service using UART | This example application demonstrates the UART based console and debug system service |
1.2 FAT File System using NVM Media | This application shows an example of implementing a FAT disk in the device internal Flash memory |
1.3 FAT File System using SDSPI Media | This application shows an example of using the FAT File System to access and modify the contents of a SD card using the SDSPI driver and the SPI PLIB |
1.4 FreeRTOS Basic | This example application demonstrates context switching between four tasks of different priorities. Two tasks run periodically while the other two tasks are event driven |
1.5 I2C Driver Asynchronous - I2C Multi-client | This example application demonstrates the multi-client feature of the asynchronous mode of the I2C driver by communicating with an external EEPROM and a temperature sensor |
1.6 I2C EEPROM Driver - AT24 EEPROM Read Write | This example application demonstrates how to use the AT24 driver to perform read and write operations on AT24 series of EEPROM |
1.7 SPI Driver Asynchronous - Self Loopback Multi Client | This example demonstrates how to use the SPI driver in asynchronous mode to achieve self-loop back between multiple clients |
1.8 SPI EEPROM Driver - AT25 EEPROM Read Write | This example application demonstrates how to use the AT25 driver to perform read and write operations on AT25 series of EEPROM |
1.9 Time System Service Multi-client | This example application demonstrates the multi-client system timer functionality |
1.10 USART Driver Synchronous - Usart Echo | This example application demonstrates the synchronous mode of the USART driver by echoing the received characters |