1.6 I2C EEPROM Driver - AT24 EEPROM Read Write

This example application demonstrates how to use the AT24 driver to perform read and write operations on AT24 series of EEPROM.

Description

This example uses the AT24 driver to communicate with the I2C based AT24 series of EEPROMs to perform read and write operations.

The application communicates with the EEPROM 3 click board that has AT24CM02 EEPROM on it.

Downloading and Building the Application

To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.

Path of the application within the repository is apps/driver/i2c_eeprom/at24/at24_eeprom_read_write/firmware.

To build the application, refer to the following table and open the project using its IDE.

Project Name Description
pic32cx_mtsh_db.X MPLABX project for PIC32CXMTSH-DB Evaluation Kit

Setting Up the Hardware

The following table shows the target hardware for the application projects.

Project Name Description
pic32cx_mtsh_db.X PIC32CXMTSH-DB Evaluation Kit

Running the Application

  1. Build and program the application using its IDE.
  2. The LED indicates the success or failure.
    • The LED is turned ON when the data read from EEPROM matches with the written data
Refer to the following table for LED name:
Board LED Name
PIC32CXMTSH-DB Evaluation Kit D20