3.1.2 Low-Voltage Programming (LVP) Mode
The LVP mode allows the devices to be programmed using VDD only, without high
voltage. When the LVP bit in the Configuration Word 4 register is set to
‘1’, the Low-Voltage ICSP Programming entry is enabled. To disable
the Low-Voltage ICSP mode, the LVP bit must be programmed to ‘0’. This
can only be done while in the High-Voltage Entry mode.
- MCLR is brought to VIL.
- A 32-bit key sequence is
presented on ICSPDAT and clocked by ICSPCLK. The Least Significant bit (LSb) of
the pattern is a ‘don’t care
X’. The Program/Verify mode entry pattern detect hardware verifies only the first 31 bits of the sequence and the last clock is required before the pattern detect goes active.
The key sequence is a specific 32-bit pattern, ‘32’h4d434850’ (more
easily remembered as MCHP in ASCII). The device will enter Program/Verify mode only if
the sequence is valid. The MSb of the Most Significant Byte (MSB) must be shifted in
first. Once the key sequence is complete, MCLR must be held at
VIL for as long as Program/Verify mode is to be maintained. For LVP
timing, see Figure 3-3 and Figure 3-4.
To enter LVP mode, the MSb of the Most Significant nibble must be shifted in first. This differs from entering the key sequence on some other device families.