4.2 Specifying Configuration Fuses
While MPLAB XC8 will accept the code used with AVR-GCC to program the fuses in the Configuration Words, it also allows the Configuration Words to be specified in a simpler way. Consider the new constructs for new or migrated projects, but do not use a mix of programming methodologies.
MPLAB XC8 uses the config pragma to specify one or more Configuration
Word setting-value pairs. The pragma ensures that the fuse data that is programmed into
the device is placed in the correct section and linked at the correct address.
#pragma config setting = value[,setting = value,...]where
setting is a fuse setting descriptor, e.g.,
WDTON, and value is a textual
description of the desired state, for example CLEAR. Those states other
than SET and CLEAR are prefixed with the setting
descriptor, as in BODLEVEL_4V3 for the 4.3 Volt
BODLEVEL setting, as shown in the following
examples:#pragma config SUT_CKSEL = SUT_CKSEL_14CK_62MS5
#pragma config BOOTRST = CLEAR, BOOTSZ = BOOTSZ_2048W_4800For assistance with the setting-value names, open the avr_chipinfo.html
file that is located in the compiler's docs directory. Click the link
to your target device and the linked page will show you the pragma settings and values
that are appropriate for your device, along with examples. Review your device data sheet
for more information on the operation of the fuses.