6.3 Info Command

The Info command accesses some static or dynamic status information from the device depending upon the parameters input to the command. The specific command modes include:
Revision
Returns a value indicating the device identification byte and the revision number of the device. It is recommended that software not depend on the revision information as it may change over time.
LockStatus
Returns a value indicating if the Slot selected in either the Configuration or Data zone is locked or unlocked. After the Delete command has been run this mode will always fail.
ChipStatus
Returns a value. The first byte returned indicates if the Delete command has been used to clear the data slots.