5.6.1 Pin Manager
I/O Port Management and Configuration
5.6.1.1 Introduction
The Mega AVR Pin Manager controls the I/O pins that represent the instances of the PORT peripheral registers. Each PORT instance has up to eight I/O pins. The PORTs are named PORTA, PORTB, PORTC, etc.
5.6.1.2 Supported Device Families
ATmega32x |
5.6.1.3 Required header files:
#include"mcc_generated_files/system/pins.h"
5.6.1.4 Module Documentation
5.6.1.4.1 Pins Driver
This file contains the API prototypes and function macros for the Pins driver.
Module description
This file contains the API prototypes and function macros for the Pins driver.
Functions
void PIN_MANAGER_Initialize ()
Initializes the General Purpose Input/Output (GPIO), peripheral I/O pins and related registers.
Function Documentation
PIN_MANAGER_Initialize()
void PIN_MANAGER_Initialize ( )
Initializes the General Purpose Input/Output (GPIO), peripheral I/O pins and related registers.
|
None. |
5.6.1.5 File Documentation
5.6.1.5.1 source/pins.c File Reference
This file contains the API implementations for the Pins driver.
#include "../pins.h"
Functions
void PIN_MANAGER_Initialize ()
Initializes the General Purpose Input/Output (GPIO), peripheral I/O pins and related registers.
Detailed Description
This file contains the API implementations for the Pins driver.
Generated Driver File
5.6.1.5.2 source/pins.h File Reference
#include <avr/io.h> #include "./port.h"
Functions
void PIN_MANAGER_Initialize ()
Initializes the General Purpose Input/Output (GPIO), peripheral I/O pins and related registers.
Macros
Pin Function Macros
These sets of macros are generated for all the selected pins in the Pins module.
#define IO_PB0_SetHigh() do { PORTB |= 0x1; } while(0)
#define IO_PB0_SetLow() do { PORTB &= ~0x1; } while(0)
#define IO_PB0_Toggle() do { PINB |= 0x1; } while(0)
#define IO_PB0_GetValue() (PINB & (0x1 << 0))
#define IO_PB0_SetDigitalInput() do { DDRB &= ~0x1; } while(0)
#define IO_PB0_SetDigitalOutput() do { DDRB |= 0x1; } while(0)
#define IO_PB0_SetPullUp() do { PORTB |= 0x1; } while(0)
#define IO_PB0_ResetPullUp() do { PORTB &= ~0x1; } while(0)
#define IO_PB1_SetHigh() do { PORTB |= 0x2; } while(0)
#define IO_PB1_SetLow() do { PORTB &= ~0x2; } while(0)
#define IO_PB1_Toggle() do { PINB |= 0x2; } while(0)
#define IO_PB1_GetValue() (PINB & (0x1 << 1))
#define IO_PB1_SetDigitalInput() do { DDRB &= ~0x2; } while(0)
#define IO_PB1_SetDigitalOutput() do { DDRB |= 0x2; } while(0)
#define IO_PB1_SetPullUp() do { PORTB |= 0x2; } while(0)
#define IO_PB1_ResetPullUp() do { PORTB &= ~0x2; } while(0)
Detailed Description
Generated Pins Header File
Macro Definition Documentation
IO_PB0_GetValue
#define IO_PB0_GetValue( ) (PINB & (0x1 << 0))
IO_PB0_ResetPullUp
#define IO_PB0_ResetPullUp( ) do { PORTB &= ~0x1; } while(0)
IO_PB0_SetDigitalInput
#define IO_PB0_SetDigitalInput( ) do { DDRB &= ~0x1; } while(0)
IO_PB0_SetDigitalOutput
#define IO_PB0_SetDigitalOutput( ) do { DDRB |= 0x1; } while(0)
IO_PB0_SetHigh
#define IO_PB0_SetHigh( ) do { PORTB |= 0x1; } while(0)
IO_PB0_SetLow
#define IO_PB0_SetLow( ) do { PORTB &= ~0x1; } while(0)
IO_PB0_SetPullUp
#define IO_PB0_SetPullUp( ) do { PORTB |= 0x1; } while(0)
IO_PB0_Toggle
#define IO_PB0_Toggle( ) do { PINB |= 0x1; } while(0)
IO_PB1_GetValue
#define IO_PB1_GetValue( ) (PINB & (0x1 << 1))
IO_PB1_ResetPullUp
#define IO_PB1_ResetPullUp( ) do { PORTB &= ~0x2; } while(0)
IO_PB1_SetDigitalInput
#define IO_PB1_SetDigitalInput( ) do { DDRB &= ~0x2; } while(0)
IO_PB1_SetDigitalOutput
#define IO_PB1_SetDigitalOutput( ) do { DDRB |= 0x2; } while(0)
IO_PB1_SetHigh
#define IO_PB1_SetHigh( ) do { PORTB |= 0x2; } while(0)
IO_PB1_SetLow
#define IO_PB1_SetLow( ) do { PORTB &= ~0x2; } while(0)
IO_PB1_SetPullUp
#define IO_PB1_SetPullUp( ) do { PORTB |= 0x2; } while(0)
IO_PB1_Toggle
#define IO_PB1_Toggle( ) do { PINB |= 0x2; } while(0)
5.6.1.5.3 source/port.h File Reference
This file contains enumerations related to the operation of the Pins driver.
#include "utils/compiler.h"
Enumerations
enum port_pull_mode { PORT_PULL_OFF, PORT_PULL_UP }
enum port_dir { PORT_DIR_IN, PORT_DIR_OUT, PORT_DIR_OFF }
Detailed Description
This file contains enumerations related to the operation of the Pins driver.
Generated Ports Header File
Enumeration Type Documentation
port_dir
enum port_dir
PORT_DIR_IN | ||
PORT_DIR_OUT | ||
PORT_DIR_OFF |
port_pull_mode
enum port_pull_mode
PORT_PULL_OFF | ||
PORT_PULL_UP |