4.3 CAN FD - Controller Area Network Flexible Data-Rate
4.3.1 Introduction
The MPLAB® Code Configurator (MCC) Melody CAN 2.0/CAN FD Peripheral Library (PLIBs) drivers generates APIs to support CAN 2.0/CAN FD-specific peripheral functionality on target MCUs. This PLIB is supported by the Melody CAN 2.0 and CAN FD Drivers. Please refer to 3.1 CAN 2.0/CAN FD Driver for more details on the portable abstract interface and use case examples.
This reference document covers implementation of the CAN FD PLIB only. The APIs supported by CAN FD and CAN 2.0 are almost similar. The additional features supported by CAN FD are mentioned wherever applicable. PIC18F-Q83 family of devices does not support CAN FD mode.
The Controller Area Network Flexible Data-Rate (CAN FD) is a two-wire data communication protocol typically used for broadcasting sensor data and control information between different parts of electronic instrumentation and control systems. This protocol is generally used in modern high performance vehicles.
4.3.2 Supported Device Families
PIC18F-Q83 | PIC18F-Q84 |
4.3.3 Required Header Files
#include "mcc_generated_files/can/can1.h"
4.3.4 Module Documentation
4.3.4.1 CAN FD DRIVER
This file contains API prototypes and other data types for the CAN1 driver.
4.3.4.1.1 Module description
This file contains API prototypes and other data types for the CAN1 driver.
Note: This reference document uses CAN1_TXQ, CAN1_FIFO_1 for transmit functionality and CAN1_FIFO_2, CAN1_FIFO_3 for receive functionality.
Data structures
struct CAN1_FIFOREG
Defines a structure to access CAN1 FIFO Registers.
struct CAN1_RX_FIFO_MSG
CAN1 Receive FIFO Message Object head count information maintenance data structure.
struct CAN_MSG_FIELD
Used to configure the message fields of CAN frame.
struct CAN_MSG_OBJ
Used to configure the message object of CAN frame.
Definitions
#define CAN_FD1_Initialize CAN1_Initialize
Defines the Custom Name for CAN1_Initialize() API.
#define CAN_FD1_Deinitialize CAN1_Deinitialize
Defines the Custom Name for CAN1_Deinitialize() API.
#define CAN_FD1_OperationModeSet CAN1_OperationModeSet
Defines the Custom Name for CAN1_OperationModeSet() API.
#define CAN_FD1_OperationModeGet CAN1_OperationModeGet
Defines the Custom Name for CAN1_OperationModeGet() API.
#define CAN_FD1_Transmit CAN1_Transmit
Defines the Custom Name for CAN1_Transmit() API.
#define CAN_FD1_TransmitFIFOStatusGet CAN1_TransmitFIFOStatusGet
Defines the Custom Name for CAN1_TransmitFIFOStatusGet() API.
#define CAN_FD1_IsTxErrorPassive CAN1_IsTxErrorPassive
Defines the Custom Name for CAN1_IsTxErrorPassive() API.
#define CAN_FD1_IsTxErrorWarning CAN1_IsTxErrorWarning
Defines the Custom Name for CAN1_IsTxErrorWarning() API.
#define CAN_FD1_IsTxErrorActive CAN1_IsTxErrorActive
Defines the Custom Name for CAN1_IsTxErrorActive() API.
#define CAN_FD1_Receive CAN1_Receive
Defines the Custom Name for CAN1_Receive() API.
#define CAN_FD1_ReceiveMessageGet CAN1_ReceiveMessageGet
Defines the Custom Name for CAN1_ReceiveMessageGet() API.
#define CAN_FD1_ReceivedMessageCountGet CAN1_ReceivedMessageCountGet
Defines the Custom Name for CAN1_ReceivedMessageCountGet() API.
#define CAN_FD1_ReceiveFIFOStatusGet CAN1_ReceiveFIFOStatusGet
Defines the Custom Name for CAN1_ReceiveFIFOStatusGet() API.
#define CAN_FD1_IsRxErrorPassive CAN1_IsRxErrorPassive
Defines the Custom Name for CAN1_IsRxErrorPassive() API.
#define CAN_FD1_IsRxErrorWarning CAN1_IsRxErrorWarning
Defines the Custom Name for CAN1_IsRxErrorWarning() API.
#define CAN_FD1_IsRxErrorActive CAN1_IsRxErrorActive
Defines the Custom Name for CAN1_IsRxErrorActive() API.
#define CAN_FD1_IsBusOff CAN1_IsBusOff
Defines the Custom Name for CAN1_IsBusOff() API.
#define CAN_FD1_Sleep CAN1_Sleep
Defines the Custom Name for CAN1_Sleep() API.
#define CAN_FD1_InvalidMessageCallbackRegister CAN1_InvalidMessageCallbackRegister
Defines the Custom Name for CAN1_InvalidMessageCallbackRegister() API.
#define CAN_FD1_BusWakeUpActivityCallbackRegister CAN1_BusWakeUpActivityCallbackRegister
Defines the Custom Name for CAN1_BusWakeUpActivityCallbackRegister() API.
#define CAN_FD1_BusErrorCallbackRegister CAN1_BusErrorCallbackRegister
Defines the Custom Name for CAN1_BusErrorCallbackRegister() API.
#define CAN_FD1_ModeChangeCallbackRegister CAN1_ModeChangeCallbackRegister
Defines the Custom Name for CAN1_ModeChangeCallbackRegister() API.
#define CAN_FD1_SystemErrorCallbackRegister CAN1_SystemErrorCallbackRegister
Defines the Custom Name for CAN1_SystemErrorCallbackRegister() API.
#define CAN_FD1_TxAttemptCallbackRegister CAN1_TxAttemptCallbackRegister
Defines the Custom Name for CAN1_TxAttemptCallbackRegister() API.
#define CAN_FD1_RxBufferOverFlowCallbackRegister CAN1_RxBufferOverFlowCallbackRegister
Defines the Custom Name for CAN1_RxBufferOverFlowCallbackRegister() API.
#define CAN1_TX_TXQ CAN1_TXQ
CAN1 Transmit FIFO TXQ Custom Name.
#define CAN1_TX_FIFO1 CAN1_FIFO_1
CAN1 Transmit FIFO 1 Custom Name.
#define CAN1_RX_FIFO2 CAN1_FIFO_2
CAN1 Receive FIFO 2 Custom Name.
#define CAN1_RX_FIFO3 CAN1_FIFO_3
CAN1 Receive FIFO 3 Custom Name.
#define CAN_FD1_Tasks CAN1_Tasks
Defines the Custom Name for CAN1_Tasks() API.
#define CAN_FD_MESSAGE_FORMAT_FEATURE_AVAILABLE 1
Defines the CAN FD Message format data update request functionality.
#define CAN_FIFO_BASED_TRANSMIT_PRIORITY_FEATURE_AVAILABLE 1
Defines the CAN FIFO based transmit priority data update request functionality.
#define CAN_DMA_INTERFACE_FEATURE_AVAILABLE 0
Defines the CAN 2.0 DMA interface data update request functionality.
Enumerations
enum CAN_TX_FIFO_CHANNELS { CAN1_TXQ = 0, CAN1_FIFO_1 = 1, CAN_TX_FIFO_MAX }
Defines the CAN FIFOs configured as transmit.
enum CAN_RX_FIFO_CHANNELS { CAN1_FIFO_2 = 2, CAN1_FIFO_3 = 3, CAN_RX_FIFO_MAX }
Defines the CAN FIFOs configured as receive.
enum CAN_MSG_OBJ_BRS_MODE { CAN_NON_BRS_MODE = 0, CAN_BRS_MODE = 1 }
Defines if the bit rate switching is enabled or disabled in the CAN message object.
enum CAN_MSG_OBJ_ID_TYPE { CAN_FRAME_STD = 0, CAN_FRAME_EXT = 1 }
Defines if the message ID is Standard ID or Extended ID in CAN message object.
enum CAN_MSG_OBJ_FRAME_TYPE { CAN_FRAME_DATA = 0, CAN_FRAME_RTR = 1 }
Defines if the frame type is Data frame or Remote Transmit Request frame in CAN message object.
enum CAN_MSG_OBJ_TYPE { CAN_2_0_FORMAT = 0, CAN_FD_FORMAT = 1 }
Defines if the CAN message object is in CAN FD format or CAN 2.0 format.
enum CAN_TX_MSG_REQUEST_STATUS { CAN_TX_MSG_REQUEST_SUCCESS = 0, CAN_TX_MSG_REQUEST_DLC_EXCEED_ERROR = 1, CAN_TX_MSG_REQUEST_BRS_ERROR = 2, CAN_TX_MSG_REQUEST_FIFO_FULL = 3 }
Defines the CAN transmit API return status.
enum CAN_OP_MODES { CAN_NORMAL_FD_MODE = 0x0, CAN_DISABLE_MODE = 0x1, CAN_INTERNAL_LOOPBACK_MODE = 0x2, CAN_LISTEN_ONLY_MODE = 0x3, CAN_CONFIGURATION_MODE = 0x4, CAN_EXTERNAL_LOOPBACK_MODE = 0x5, CAN_NORMAL_2_0_MODE = 0x6, CAN_RESTRICTED_OPERATION_MODE =0x7 }
Defines the CAN operation modes that are available for the module to use.
enum CAN_OP_MODE_STATUS { CAN_OP_MODE_REQUEST_SUCCESS, CAN_OP_MODE_REQUEST_FAIL, CAN_OP_MODE_SYS_ERROR_OCCURED }
Defines the return status of CAN operation mode set API.
enum CAN_TX_FIFO_STATUS { CAN_TX_FIFO_FULL = 0x0, CAN_TX_FIFO_AVAILABLE = 0x1 }
Defines the status of CAN FD transmit FIFO.
enum CAN_RX_FIFO_STATUS { CAN_RX_MSG_NOT_AVAILABLE = 0x0, CAN_RX_MSG_AVAILABLE = 0x1, CAN_RX_MSG_OVERFLOW = 0x8 }
Defines the CAN FD receive FIFO status bit mask values.
enum CAN_DLC { DLC_0, DLC_1, DLC_2, DLC_3, DLC_4, DLC_5, DLC_6, DLC_7, DLC_8, DLC_12, DLC_16, DLC_20, DLC_24, DLC_32, DLC_48, DLC_64 }
Defines the CAN message payload sizes that are available for the mode to use.
Functions
static uint8_t CAN1_DlcToDataBytesGet (const enum CAN_DLC dlc)
Get the DLC enum based data byte value.
static uint8_t CAN1_PLSIZEToPayloadBytesGet (uint8_t plsize)
Get the Payload size in bytes for PLSIZE register value.
static bool CAN1_IsTxChannel (uint8_t channel)
Check if a valid channel is configured as transmitter or not.
static enum CAN_TX_FIFO_STATUS CAN1_GetTxFifoStatus (uint8_t validChannel)
Returns the CAN1 transmit FIFO status.
static void CAN1_MessageWriteToFifo (uint8_t *txFifoObj, struct CAN_MSG_OBJ *txCanMsg)
Reads the message object from user input and updates the CAN1 TX FIFO.
static enum CAN_TX_MSG_REQUEST_STATUS CAN1_ValidateTransmission (uint8_t channel, struct CAN_MSG_OBJ *txCanMsg)
Validates transmission.
static void CAN1_RX_FIFO_ResetInfo (void)
Resets the CAN1 receive message head count.
static bool CAN1_IsRxChannel (uint8_t channel)
Checks if a valid channel is configured as receiver or not.
static uint8_t CAN1_GetRxFifoStatus (uint8_t validChannel)
Returns the CAN1 Receive FIFO status.
static uint8_t CAN1_GetRxFifoDepth (uint8_t validChannel)
Returns the CAN1 Receive FIFO depth.
static void CAN1_MessageReadFromFifo (uint8_t *rxFifoObj, struct CAN_MSG_OBJ *rxCanMsg)
Reads the message object from Receive FIFO and updates the user message object.
static bool CAN1_ReceiveFromFiFo (uint8_t index, enum CAN_RX_FIFO_CHANNELS channel, struct CAN_MSG_OBJ *rxCanMsg)
Reads the data object from a particular CAN receive FIFO.
static void CAN1_TX_FIFO_Configuration (void)
Configures the CAN1 TX FIFO settings.
static void CAN1_RX_FIFO_Configuration (void)
Configures the CAN1 Receive FIFO settings.
static void CAN1_RX_FIFO_FilterMaskConfiguration (void)
Configures the CAN1 RX FIFO filter and mask settings.
static void CAN1_BitRateConfiguration (void)
Configures the CAN1 Bit rate settings.
static void CAN1_ErrorNotificationEnable (void)
Enables the CAN1 error notification interrupt.
void CAN1_Initialize (void)
Initializes the CAN1 module.
void CAN1_Deinitialize (void)
Resets the CAN1 registers and settings to their POR values.
enum CAN_OP_MODE_STATUS CAN1_OperationModeSet (const enum CAN_OP_MODES requestMode)
Sets the CAN1 Operation mode.
enum CAN_OP_MODES CAN1_OperationModeGet (void)
Gets the CAN1 Operation mode.
enum CAN_TX_MSG_REQUEST_STATUS CAN1_Transmit (const enum CAN_TX_FIFO_CHANNELS fifoChannel, struct CAN_MSG_OBJ *txCanMsg)
Writes the CAN message object to the specified transmit FIFO channel.
enum CAN_TX_FIFO_STATUS CAN1_TransmitFIFOStatusGet (const enum CAN_TX_FIFO_CHANNELS fifoChannel)
Returns the CAN1 transmitter FIFO status.
bool CAN1_IsTxErrorPassive (void)
Returns the Transmit Error Passive state. If the Transmit Error Counter is above 127, then the transmitter is in Error Passive state.
bool CAN1_IsTxErrorWarning (void)
Returns the Transmit Error Warning state. If the Transmit Error Counter is above 95 and below 128, then the transmitter is in Error Warning state.
bool CAN1_IsTxErrorActive (void)
Returns the Transmit Error Active state. If the Transmit Error Counter is above 0 and below 128, then the transmitter is in Error Active state.
bool CAN1_Receive (struct CAN_MSG_OBJ *rxCanMsg)
Reads a message object.
bool CAN1_ReceiveMessageGet (const enum CAN_RX_FIFO_CHANNELS fifoChannel, struct CAN_MSG_OBJ *rxCanMsg)
Reads a message object from the selected CAN1 receive FIFO.
uint8_t CAN1_ReceivedMessageCountGet (void)
Returns the number of CAN messages received in all the FIFOs.
uint8_t CAN1_ReceiveFIFOStatusGet (const enum CAN_RX_FIFO_CHANNELS fifoChannel)
Returns the CAN1 receiver FIFO status.
bool CAN1_IsRxErrorPassive (void)
Returns the Receive Error Passive state. If the Receive Error Counter is above 127, then the receiver is in Error Passive state.
bool CAN1_IsRxErrorWarning (void)
Returns the Receive Error Warning state. If the Receive Error Counter is above 95 and below 128, then the receiver is in Error Warning state.
bool CAN1_IsRxErrorActive (void)
Returns the Receive Error Active state. If the Receive Error Counter is above 0 and below 128, then the receiver is in Error Active state.
bool CAN1_IsBusOff (void)
Returns the Bus Off status.
void CAN1_Sleep (void)
Puts the CAN1 node into Sleep mode.
void CAN1_InvalidMessageCallbackRegister (void(*handler)(void))
Setter function for the CAN1_InvalidMessage callback.
void CAN1_BusWakeUpActivityCallbackRegister (void(*handler)(void))
Setter function for the CAN1_BusWakeUpActivity callback.
void CAN1_BusErrorCallbackRegister (void(*handler)(void))
Setter function for the CAN1_BusError callback.
void CAN1_ModeChangeCallbackRegister (void(*handler)(void))
Setter function for the CAN1_ModeChange callback.
void CAN1_SystemErrorCallbackRegister (void(*handler)(void))
Setter function for the CAN1_SystemError callback.
void CAN1_TxAttemptCallbackRegister (void(*handler)(void))
Setter function for the CAN1_TxAttempt callback.
void CAN1_RxBufferOverFlowCallbackRegister (void(*handler)(void))
Setter function for the CAN1_RxBufferOverFlow callback.
void CAN1_TXQEmptyCallbackRegister (void(*handler)(void))
Setter function for the CAN1_TXQEmpty callback.
void CAN1_FIFO1HalfEmptyCallbackRegister (void(*handler)(void))
Setter function for the CAN1_FIFO1HalfEmpty callback.
void CAN1_FIFO2NotEmptyCallbackRegister (void(*handler)(void))
Setter function for the CAN1_FIFO2NotEmpty callback.
void CAN1_FIFO3FullCallbackRegister (void(*handler)(void))
Setter function for the CAN1_FIFO3Full callback.
void CAN1_Tasks (void)
Used to implement the tasks for polled implementations.
Variables
const struct CAN_INTERFACE CAN_FD1
Structure object of type CAN_INTERFACE with the custom name given by the user.
4.3.4.1.2 Definition Documentation
CAN1_RX_FIFO2
#define CAN1_RX_FIFO2 CAN1_FIFO_2
CAN1 Receive FIFO 2 Custom Name.
Defines the custom name of CAN1_FIFO_2 used for Receive functionality.
CAN1_RX_FIFO3
#define CAN1_RX_FIFO3 CAN1_FIFO_3
CAN1 Receive FIFO 3 Custom Name.
Defines the custom name of CAN1_FIFO_3 used for Receive functionality.
CAN1_TX_FIFO1
#define CAN1_TX_FIFO1 CAN1_FIFO_1
CAN1 Transmit FIFO 1 Custom Name.
Defines the custom name of CAN1_FIFO_1 used for Transmit functionality.
CAN1_TX_TXQ
#define CAN1_TX_TXQ CAN1_TXQ
CAN1 Transmit FIFO TXQ Custom Name.
Defines the custom name of CAN1_TXQ used for Transmit functionality.
CAN_DMA_INTERFACE_FEATURE_AVAILABLE
#define CAN_DMA_INTERFACE_FEATURE_AVAILABLE 0
Defines the CAN 2.0 DMA interface data update request functionality.
CAN_FD1_BusErrorCallbackRegister
#define CAN_FD1_BusErrorCallbackRegister CAN1_BusErrorCallbackRegister
Defines the Custom Name for CAN1_BusErrorCallbackRegister() API.
CAN_FD1_BusWakeUpActivityCallbackRegister
#define CAN_FD1_BusWakeUpActivityCallbackRegister CAN1_BusWakeUpActivityCallbackRegister
Defines the Custom Name for CAN1_BusWakeUpActivityCallbackRegister() API.
CAN_FD1_Deinitialize
#define CAN_FD1_Deinitialize CAN1_Deinitialize
Defines the Custom Name for CAN1_Deinitialize() API.
CAN_FD1_Initialize
#define CAN_FD1_Initialize CAN1_Initialize
Defines the Custom Name for CAN1_Initialize() API.
CAN_FD1_InvalidMessageCallbackRegister
#define CAN_FD1_InvalidMessageCallbackRegister CAN1_InvalidMessageCallbackRegister
Defines the Custom Name for CAN1_InvalidMessageCallbackRegister() API.
CAN_FD1_IsBusOff
#define CAN_FD1_IsBusOff CAN1_IsBusOff
Defines the Custom Name for CAN1_IsBusOff() API.
CAN_FD1_IsRxErrorActive
#define CAN_FD1_IsRxErrorActive CAN1_IsRxErrorActive
Defines the Custom Name for CAN1_IsRxErrorActive() API.
CAN_FD1_IsRxErrorPassive
#define CAN_FD1_IsRxErrorPassive CAN1_IsRxErrorPassive
Defines the Custom Name for CAN1_IsRxErrorPassive() API.
CAN_FD1_IsRxErrorWarning
#define CAN_FD1_IsRxErrorWarning CAN1_IsRxErrorWarning
Defines the Custom Name for CAN1_IsRxErrorWarning() API.
CAN_FD1_IsTxErrorActive
#define CAN_FD1_IsTxErrorActive CAN1_IsTxErrorActive
Defines the Custom Name for CAN1_IsTxErrorActive() API.
CAN_FD1_IsTxErrorPassive
#define CAN_FD1_IsTxErrorPassive CAN1_IsTxErrorPassive
Defines the Custom Name for CAN1_IsTxErrorPassive() API.
CAN_FD1_IsTxErrorWarning
#define CAN_FD1_IsTxErrorWarning CAN1_IsTxErrorWarning
Defines the Custom Name for CAN1_IsTxErrorWarning() API.
CAN_FD1_ModeChangeCallbackRegister
#define CAN_FD1_ModeChangeCallbackRegister CAN1_ModeChangeCallbackRegister
Defines the Custom Name for CAN1_ModeChangeCallbackRegister() API.
CAN_FD1_OperationModeGet
#define CAN_FD1_OperationModeGet CAN1_OperationModeGet
Defines the Custom Name for CAN1_OperationModeGet() API.
CAN_FD1_OperationModeSet
#define CAN_FD1_OperationModeSet CAN1_OperationModeSet
Defines the Custom Name for CAN1_OperationModeSet() API.
CAN_FD1_Receive
#define CAN_FD1_Receive CAN1_Receive
Defines the Custom Name for CAN1_Receive() API.
CAN_FD1_ReceivedMessageCountGet
#define CAN_FD1_ReceivedMessageCountGet CAN1_ReceivedMessageCountGet
Defines the Custom Name for CAN1_ReceivedMessageCountGet() API.
CAN_FD1_ReceiveFIFOStatusGet
#define CAN_FD1_ReceiveFIFOStatusGet CAN1_ReceiveFIFOStatusGet
Defines the Custom Name for CAN1_ReceiveFIFOStatusGet() API.
CAN_FD1_ReceiveMessageGet
#define CAN_FD1_ReceiveMessageGet CAN1_ReceiveMessageGet
Defines the Custom Name for CAN1_ReceiveMessageGet() API.
CAN_FD1_RxBufferOverFlowCallbackRegister
#define CAN_FD1_RxBufferOverFlowCallbackRegister CAN1_RxBufferOverFlowCallbackRegister
Defines the Custom Name for CAN1_RxBufferOverFlowCallbackRegister() API.
CAN_FD1_Sleep
#define CAN_FD1_Sleep CAN1_Sleep
Defines the Custom Name for CAN1_Sleep() API.
CAN_FD1_SystemErrorCallbackRegister
#define CAN_FD1_SystemErrorCallbackRegister CAN1_SystemErrorCallbackRegister
Defines the Custom Name for CAN1_SystemErrorCallbackRegister() API.
CAN_FD1_Tasks
#define CAN_FD1_Tasks CAN1_Tasks
Defines the Custom Name for CAN1_Tasks() API.
CAN_FD1_Transmit
#define CAN_FD1_Transmit CAN1_Transmit
Defines the Custom Name for CAN1_Transmit() API.
CAN_FD1_TransmitFIFOStatusGet
#define CAN_FD1_TransmitFIFOStatusGet CAN1_TransmitFIFOStatusGet
Defines the Custom Name for CAN1_TransmitFIFOStatusGet() API.
CAN_FD1_TxAttemptCallbackRegister
#define CAN_FD1_TxAttemptCallbackRegister CAN1_TxAttemptCallbackRegister
Defines the Custom Name for CAN1_TxAttemptCallbackRegister() API.
CAN_FD_MESSAGE_FORMAT_FEATURE_AVAILABLE
#define CAN_FD_MESSAGE_FORMAT_FEATURE_AVAILABLE 1
Defines the CAN FD Message format data update request functionality.
APIs Supported: CAN_TX_MSG_REQUEST_STATUS CANx_Transmit(const CANx_TX_FIFO_CHANNELS fifoChannel, CAN_MSG_OBJ *txCanMsg); bool CANx_Receive(CAN_MSG_OBJ *rxCanMsg);
CAN_FIFO_BASED_TRANSMIT_PRIORITY_FEATURE_AVAILABLE
#define CAN_FIFO_BASED_TRANSMIT_PRIORITY_FEATURE_AVAILABLE 1
Defines the CAN FIFO based transmit priority data update request functionality.
APIs Supported: CAN_TX_MSG_REQUEST_STATUS CANx_Transmit(const CANx_TX_FIFO_CHANNELS fifoChannel, CAN_MSG_OBJ *txCanMsg); CAN_TX_FIFO_STATUS CANx_TransmitFIFOStatusGet(const CANx_TX_FIFO_CHANNELS fifoChannel);
4.3.4.1.3 Function Documentation
CAN1_BitRateConfiguration()
static void CAN1_BitRateConfiguration (void )[static]
Configures the CAN1 Bit rate settings.
None. |
None. |
CAN1_BusErrorCallbackRegister()
void CAN1_BusErrorCallbackRegister (void (*handler)(void))
Setter function for the CAN1_BusError callback.
in | handler |
- Pointer to the callback routine. |
None. |
CAN1_BusWakeUpActivityCallbackRegister()
void CAN1_BusWakeUpActivityCallbackRegister (void (*handler)(void))
Setter function for the CAN1_BusWakeUpActivity callback.
in | handler |
- Pointer to the callback routine. |
None. |
CAN1_Deinitialize()
void CAN1_Deinitialize (void )
Resets the CAN1 registers and settings to their POR values.
None. |
None. |
CAN1_DlcToDataBytesGet()
static uint8_t CAN1_DlcToDataBytesGet (const enum CAN_DLC dlc)[static]
Get the DLC enum based data byte value.
in | dlc |
- DLC value as described in CAN_DLC. |
The data byte value coresponding to DLC. |
CAN1_ErrorNotificationEnable()
static void CAN1_ErrorNotificationEnable (void )[static]
Enables the CAN1 error notification interrupt.
None. |
None. |
CAN1_FIFO1HalfEmptyCallbackRegister()
void CAN1_FIFO1HalfEmptyCallbackRegister (void (*handler)(void))
Setter function for the CAN1_FIFO1HalfEmpty callback.
in | handler |
- Pointer to the callback routine. |
None. |
CAN1_FIFO2NotEmptyCallbackRegister()
void CAN1_FIFO2NotEmptyCallbackRegister (void (*handler)(void))
Setter function for the CAN1_FIFO2NotEmpty callback.
in | handler |
- Pointer to the callback routine. |
None. |
CAN1_FIFO3FullCallbackRegister()
void CAN1_FIFO3FullCallbackRegister (void (*handler)(void))
Setter function for the CAN1_FIFO3Full callback.
in | handler |
- Pointer to the callback routine. |
None. |
CAN1_GetRxFifoDepth()
static uint8_t CAN1_GetRxFifoDepth (uint8_t validChannel)[static]
Returns the CAN1 Receive FIFO depth.
in | validChannel |
- Receive FIFO channel as described in CAN_RX_FIFO_CHANNELS. |
Depth of the Receive FIFO. |
CAN1_GetRxFifoStatus()
static uint8_t CAN1_GetRxFifoStatus (uint8_t validChannel)[static]
Returns the CAN1 Receive FIFO status.
in | validChannel |
- Receive FIFO channel as described in CAN_RX_FIFO_CHANNELS. |
Status of the CAN1 Receive FIFO. Refer CAN_RX_FIFO_STATUS for details. |
CAN1_GetTxFifoStatus()
static enum CAN_TX_FIFO_STATUS CAN1_GetTxFifoStatus (uint8_t validChannel)[static]
Returns the CAN1 transmit FIFO status.
in | channel |
- Transmit FIFO channel as described in CAN_TX_FIFO_CHANNELS. |
Status of the CAN1 Transmit FIFO as described in CAN_TX_FIFO_STATUS. |
CAN1_Initialize()
void CAN1_Initialize (void )
Initializes the CAN1 module.
None. |
None. |
CAN1_InvalidMessageCallbackRegister()
void CAN1_InvalidMessageCallbackRegister (void (*handler)(void))
Setter function for the CAN1_InvalidMessage callback.
in | handler |
- Pointer to the callback routine. |
None. |
CAN1_IsBusOff()
bool CAN1_IsBusOff (void )
Returns the Bus Off status.
CAN1_Initialize() function is already called. |
None. |
True |
- CAN1 node is in Bus Off state. |
False |
- CAN1 node is not in Bus Off state. |
CAN1_IsRxChannel()
static bool CAN1_IsRxChannel (uint8_t channel)[static]
Checks if a valid channel is configured as receiver or not.
in | channel |
- Receive FIFO channel as described in CAN_RX_FIFO_CHANNELS. |
True |
- FIFO channel is configured as receiver. |
False |
- FIFO channel is not configured as receiver. |
CAN1_IsRxErrorActive()
bool CAN1_IsRxErrorActive (void )
Returns the Receive Error Active state. If the Receive Error Counter is above 0 and below 128, then the receiver is in Error Active state.
CAN1_Initialize() function is already called. |
None. |
True |
- CAN1 node is in Receive Error Active state. |
False |
- CAN1 node is not in Receive Error Active state. |
CAN1_IsRxErrorPassive()
bool CAN1_IsRxErrorPassive (void )
Returns the Receive Error Passive state. If the Receive Error Counter is above 127, then the receiver is in Error Passive state.
CAN1_Initialize() function is already called. |
None. |
True |
- CAN1 node is in Receive Error Passive state. |
False |
- CAN1 node is not in Receive Error Passive state. |
CAN1_IsRxErrorWarning()
bool CAN1_IsRxErrorWarning (void )
Returns the Receive Error Warning state. If the Receive Error Counter is above 95 and below 128, then the receiver is in Error Warning state.
CAN1_Initialize() function is already called. |
None. |
True |
- CAN1 node is in Receive Error Warning state. |
False |
- CAN1 node is not in Receive Error Warning state. |
CAN1_IsTxChannel()
static bool CAN1_IsTxChannel (uint8_t channel)[static]
Check if a valid channel is configured as transmitter or not.
in | channel |
- Transmit FIFO channel as described in CAN_TX_FIFO_CHANNELS. |
True |
- FIFO channel is configured as transmitter. |
False |
- FIFO channel is not configured as transmitter. |
CAN1_IsTxErrorActive()
bool CAN1_IsTxErrorActive (void )
Returns the Transmit Error Active state. If the Transmit Error Counter is above 0 and below 128, then the transmitter is in Error Active state.
CAN1_Initialize() function is already called. |
None. |
True |
- CAN1 node is in Transmit Error Active state. |
False |
- CAN1 node is not in Transmit Error Active state. |
CAN1_IsTxErrorPassive()
bool CAN1_IsTxErrorPassive (void )
Returns the Transmit Error Passive state. If the Transmit Error Counter is above 127, then the transmitter is in Error Passive state.
CAN1_Initialize() function is already called. |
None. |
True |
- CAN1 node is in Transmit Error Passive state. |
False |
- CAN1 node is not in Transmit Error Passive state. |
CAN1_IsTxErrorWarning()
bool CAN1_IsTxErrorWarning (void )
Returns the Transmit Error Warning state. If the Transmit Error Counter is above 95 and below 128, then the transmitter is in Error Warning state.
CAN1_Initialize() function is already called. |
None. |
True |
- CAN1 node is in Transmit Error Warning state. |
False |
- CAN1 node is not in Transmit Error Warning state. |
CAN1_MessageReadFromFifo()
static void CAN1_MessageReadFromFifo (uint8_t * rxFifoObj, struct CAN_MSG_OBJ * rxCanMsg)[static]
Reads the message object from Receive FIFO and updates the user message object.
in | rxFifoObj |
- Receive FIFO message object. |
out | rxCanMsg |
- Pointer to the message object of type CAN_MSG_OBJ. |
None. |
CAN1_MessageWriteToFifo()
static void CAN1_MessageWriteToFifo (uint8_t * txFifoObj, struct CAN_MSG_OBJ * txCanMsg)[static]
Reads the message object from user input and updates the CAN1 TX FIFO.
out | txFifoObj |
- Transmit FIFO message object. |
in | txCanMsg |
- Pointer to the message object of type CAN_MSG_OBJ. |
None. |
CAN1_ModeChangeCallbackRegister()
void CAN1_ModeChangeCallbackRegister (void (*handler)(void))
Setter function for the CAN1_ModeChange callback.
in | handler |
- Pointer to the callback routine. |
None. |
CAN1_OperationModeGet()
enum CAN_OP_MODES CAN1_OperationModeGet (void )
Gets the CAN1 Operation mode.
CAN1_Initialize() function is already called. |
None. |
The present CAN1 Operation mode as described in CAN_OP_MODES. |
CAN1_OperationModeSet()
enum CAN_OP_MODE_STATUS CAN1_OperationModeSet (const enum CAN_OP_MODES requestMode)
Sets the CAN1 Operation mode.
CAN1_Initialize() function is already called. |
in | requestMode |
- CAN1 Operation mode as described in CAN_OP_MODES. |
Status of request to set the CAN1 Operation mode as described in CAN_OP_MODE_STATUS. |
CAN1_PLSIZEToPayloadBytesGet()
static uint8_t CAN1_PLSIZEToPayloadBytesGet (uint8_t plsize)[static]
Get the Payload size in bytes for PLSIZE register value.
in | plsize |
- The value in PLSIZE register. |
The number of data bytes corresponding to PLSIZE register value. |
CAN1_Receive()
bool CAN1_Receive (struct CAN_MSG_OBJ * rxCanMsg)
Reads a message object.
CAN1_Initialize() function is already called. The CAN1_ReceivedMessageCountGet() function is called to check if any CAN message is received. |
out | rxCanMsg |
- Pointer to the message object of type CAN_MSG_OBJ. |
True |
- CAN1 message read succeeded. |
False |
- CAN1 message read failed. |
CAN1_ReceivedMessageCountGet()
uint8_t CAN1_ReceivedMessageCountGet (void )
Returns the number of CAN messages received in all the FIFOs.
CAN1_Initialize() function is already called. |
None. |
Number of messages received. |
CAN1_ReceiveFIFOStatusGet()
uint8_t CAN1_ReceiveFIFOStatusGet (const enum CAN_RX_FIFO_CHANNELS fifoChannel)
Returns the CAN1 receiver FIFO status.
CAN1_Initialize() function is already called. |
in | fifoChannel |
- Receive FIFO channel as described in CAN_RX_FIFO_CHANNELS. |
Status of the CAN1 Receive FIFO. Refer to CAN_RX_FIFO_STATUS for details. |
CAN1_ReceiveFromFiFo()
static bool CAN1_ReceiveFromFiFo (uint8_t index, enum CAN_RX_FIFO_CHANNELS channel, struct CAN_MSG_OBJ * rxCanMsg)[static]
Reads the data object from a particular CAN receive FIFO.
in | index |
- Instance of Receive FIFO. |
in | channel |
- Receive FIFO channel as described in CAN_RX_FIFO_CHANNELS. |
out | rxCanMsg |
- Pointer to the message object of type CAN_MSG_OBJ. |
True |
- CAN1 message read succeeded. |
False |
- CAN1 message read failed. |
CAN1_ReceiveMessageGet()
bool CAN1_ReceiveMessageGet (const enum CAN_RX_FIFO_CHANNELS fifoChannel, struct CAN_MSG_OBJ * rxCanMsg)
Reads a message object from the selected CAN1 receive FIFO.
CAN1_Initialize() function is already called. The CAN1_ReceiveFIFOStatusGet() function is called to check the status of the respective CAN1 receive FIFO. |
in | fifoChannel |
- Receive FIFO channel as described in CAN_RX_FIFO_CHANNELS from where the message object is to be read. |
out | rxCanMsg |
- Pointer to the message object of type CAN_MSG_OBJ. |
True |
- CAN1 message read succeeded. |
False |
- CAN1 message read failed. |
CAN1_RX_FIFO_Configuration()
static void CAN1_RX_FIFO_Configuration (void )[static]
Configures the CAN1 Receive FIFO settings.
None. |
None. |
CAN1_RX_FIFO_FilterMaskConfiguration()
static void CAN1_RX_FIFO_FilterMaskConfiguration (void )[static]
Configures the CAN1 RX FIFO filter and mask settings.
None. |
None. |
CAN1_RX_FIFO_ResetInfo()
static void CAN1_RX_FIFO_ResetInfo (void )[static]
Resets the CAN1 receive message head count.
None. |
None. |
CAN1_RxBufferOverFlowCallbackRegister()
void CAN1_RxBufferOverFlowCallbackRegister (void (*handler)(void))
Setter function for the CAN1_RxBufferOverFlow callback.
in | handler |
- Pointer to the callback routine. |
None. |
CAN1_Sleep()
void CAN1_Sleep (void )
Puts the CAN1 node into Sleep mode.
CAN1_Initialize() function is already called. |
None. |
None. |
CAN1_SystemErrorCallbackRegister()
void CAN1_SystemErrorCallbackRegister (void (*handler)(void))
Setter function for the CAN1_SystemError callback.
in | handler |
- Pointer to the callback routine. |
None. |
CAN1_Tasks()
void CAN1_Tasks (void )
Used to implement the tasks for polled implementations.
CAN1_Initialize() function is already called. |
None. |
None. |
CAN1_Transmit()
enum CAN_TX_MSG_REQUEST_STATUS CAN1_Transmit (const enum CAN_TX_FIFO_CHANNELS fifoChannel, struct CAN_MSG_OBJ * txCanMsg)
Writes the CAN message object to the specified transmit FIFO channel.
CAN1_Initialize() function is already called. CAN1_TransmitFIFOStatusGet function is called to check buffer availability in the Transmit FIFO. |
in | fifoChannel |
- Transmit FIFO channel as described in CAN_TX_FIFO_CHANNELS where the message object is to be written. |
in | txCanMsg |
- Pointer to the message object of type CAN_MSG_OBJ. |
Status of the CAN1 Transmit operation as described in CAN_TX_MSG_REQUEST_STATUS. |
CAN1_TransmitFIFOStatusGet()
enum CAN_TX_FIFO_STATUS CAN1_TransmitFIFOStatusGet (const enum CAN_TX_FIFO_CHANNELS fifoChannel)
Returns the CAN1 transmitter FIFO status.
CAN1_Initialize() function is already called. |
in | fifoChannel |
- Transmit FIFO channel as described in CAN_TX_FIFO_CHANNELS. |
Status of the CAN1 Transmit FIFO as described in CAN_TX_FIFO_STATUS. |
CAN1_TX_FIFO_Configuration()
static void CAN1_TX_FIFO_Configuration (void )[static]
Configures the CAN1 TX FIFO settings.
None. |
None. |
CAN1_TxAttemptCallbackRegister()
void CAN1_TxAttemptCallbackRegister (void (*handler)(void))
Setter function for the CAN1_TxAttempt callback.
in | handler |
- Pointer to the callback routine. |
None. |
CAN1_TXQEmptyCallbackRegister()
void CAN1_TXQEmptyCallbackRegister (void (*handler)(void))
Setter function for the CAN1_TXQEmpty callback.
in | handler |
- Pointer to the callback routine. |
None. |
CAN1_ValidateTransmission()
static enum CAN_TX_MSG_REQUEST_STATUS CAN1_ValidateTransmission (uint8_t channel, struct CAN_MSG_OBJ * txCanMsg)[static]
Validates transmission.
in | channel |
- Transmit FIFO channel as described in CAN_TX_FIFO_CHANNELS. |
in | txCanMsg |
- Pointer to the message object of type CAN_MSG_OBJ. |
Status of the CAN1 Transmit operation as described in CAN_TX_MSG_REQUEST_STATUS. |
4.3.4.1.4 Enumeration Type Documentation
CAN_DLC
enum CAN_DLC
Defines the CAN message payload sizes that are available for the mode to use.
DLC_0 |
Data length count 0 |
DLC_1 |
Data length count 1 |
DLC_2 |
Data length count 2 |
DLC_3 |
Data length count 3 |
DLC_4 |
Data length count 4 |
DLC_5 |
Data length count 5 |
DLC_6 |
Data length count 6 |
DLC_7 |
Data length count 7 |
DLC_8 |
Data length count 8 |
DLC_12 |
Data length count 12 (Supported only in CAN FD mode) |
DLC_16 |
Data length count 16 (Supported only in CAN FD mode) |
DLC_20 |
Data length count 20 (Supported only in CAN FD mode) |
DLC_24 |
Data length count 24 (Supported only in CAN FD mode) |
DLC_32 |
Data length count 32 (Supported only in CAN FD mode) |
DLC_48 |
Data length count 48 (Supported only in CAN FD mode) |
DLC_64 |
Data length count 64 (Supported only in CAN FD mode) |
CAN_MSG_OBJ_BRS_MODE
enum CAN_MSG_OBJ_BRS_MODE
Defines if the bit rate switching is enabled or disabled in the CAN message object.
CAN_NON_BRS_MODE |
Disable BRS Mode (Supported only in CAN FD mode) |
CAN_BRS_MODE |
Enable BRS Mode (Supported only in CAN FD mode) |
CAN_MSG_OBJ_FRAME_TYPE
enum CAN_MSG_OBJ_FRAME_TYPE
Defines if the frame type is Data frame or Remote Transmit Request frame in CAN message object.
CAN_FRAME_DATA |
Data Frame CAN message object |
CAN_FRAME_RTR |
Remote Transmit Request Frame CAN message object (Supported only in CAN 2.0 mode) |
CAN_MSG_OBJ_ID_TYPE
enum CAN_MSG_OBJ_ID_TYPE
Defines if the message ID is Standard ID or Extended ID in CAN message object.
CAN_FRAME_STD |
Standard ID CAN message object |
CAN_FRAME_EXT |
Extended ID CAN message object |
CAN_MSG_OBJ_TYPE
enum CAN_MSG_OBJ_TYPE
Defines if the CAN message object is in CAN FD format or CAN 2.0 format.
CAN_2_0_FORMAT |
CAN 2.0 Message format |
CAN_FD_FORMAT |
CAN FD Message format (Supported only in CAN FD mode) |
CAN_OP_MODE_STATUS
enum CAN_OP_MODE_STATUS
Defines the return status of CAN operation mode set API.
CAN_OP_MODE_REQUEST_SUCCESS |
The requested operation mode set successfully |
CAN_OP_MODE_REQUEST_FAIL |
The requested operation mode set failure |
CAN_OP_MODE_SYS_ERROR_OCCURED |
The system error occurred while setting operation mode. |
CAN_OP_MODES
enum CAN_OP_MODES
Defines the CAN operation modes that are available for the module to use.
CAN_NORMAL_FD_MODE |
CAN FD Normal Operation Mode (Supported only in CAN FD mode) |
CAN_DISABLE_MODE |
CAN Disable Operation Mode |
CAN_INTERNAL_LOOPBACK_MODE |
CAN Internal Loopback Operation Mode |
CAN_LISTEN_ONLY_MODE |
CAN Listen only Operation Mode |
CAN_CONFIGURATION_MODE |
CAN Configuration Operation Mode |
CAN_EXTERNAL_LOOPBACK_MODE |
CAN External Loopback Operation Mode |
CAN_NORMAL_2_0_MODE |
CAN 2.0 Operation Mode |
CAN_RESTRICTED_OPERATION_MODE |
CAN Restricted Operation Mode |
CAN_RX_FIFO_CHANNELS
enum CAN_RX_FIFO_CHANNELS
Defines the CAN FIFOs configured as receive.
CAN1_FIFO_2 |
CAN1 Receive FIFO 2 |
CAN1_FIFO_3 |
CAN1 Receive FIFO 3 |
CAN_RX_FIFO_MAX |
This is added to avoid empty enum |
CAN_RX_FIFO_STATUS
enum CAN_RX_FIFO_STATUS
Defines the CAN FD receive FIFO status bit mask values.
CAN_RX_MSG_NOT_AVAILABLE |
Message is not available in receive FIFO |
CAN_RX_MSG_AVAILABLE |
Message is available in receive FIFO |
CAN_RX_MSG_OVERFLOW |
Receive FIFO has overflowed |
CAN_TX_FIFO_CHANNELS
enum CAN_TX_FIFO_CHANNELS
Defines the CAN FIFOs configured as transmit.
CAN1_TXQ |
CAN1 Transmit FIFO TXQ |
CAN1_FIFO_1 |
CAN1 Transmit FIFO 1 |
CAN_TX_FIFO_MAX |
This is added to avoid empty enum |
CAN_TX_FIFO_STATUS
enum CAN_TX_FIFO_STATUS
Defines the status of CAN FD transmit FIFO.
CAN_TX_FIFO_FULL |
Transmit FIFO is full |
CAN_TX_FIFO_AVAILABLE |
Transmit FIFO is available |
CAN_TX_MSG_REQUEST_STATUS
enum CAN_TX_MSG_REQUEST_STATUS
Defines the CAN transmit API return status.
CAN_TX_MSG_REQUEST_SUCCESS |
Transmit message object successfully placed into Transmit FIFO |
CAN_TX_MSG_REQUEST_DLC_EXCEED_ERROR |
Transmit message object DLC size is more than the Transmit FIFO configured DLC size |
CAN_TX_MSG_REQUEST_BRS_ERROR |
Transmit FIFO is configured as Non BRS mode and CAN TX Message object has BRS enabled |
CAN_TX_MSG_REQUEST_FIFO_FULL |
Transmit FIFO is Full |
4.3.4.1.5 Variable Documentation
CAN_FD1
const struct CAN_INTERFACE CAN_FD1
Structure object of type CAN_INTERFACE with the custom name given by the user.
4.3.5 Class Documentation
4.3.5.1 CAN1_FIFOREG Struct Reference
Defines a structure to access CAN1 FIFO Registers.
4.3.5.1.1 Detailed Description
Defines a structure to access CAN1 FIFO Registers.
Public Attributes
4.3.5.1.2 Member Data Documentation
The documentation for this struct was generated from the following files:
source/
source/
CONH
uint8_t CONH
CONL
uint8_t CONL
CONT
uint8_t CONT
CONU
uint8_t CONU
STAH
uint8_t STAH
STAL
uint8_t STAL
STAT
uint8_t STAT
STAU
uint8_t STAU
UA
uint32_t UA
4.3.5.2 CAN1_RX_FIFO_MSG Struct Reference
CAN1 Receive FIFO Message Object head count information maintenance data structure.
4.3.5.2.1 Detailed Description
CAN1 Receive FIFO Message Object head count information maintenance data structure.
Public Attributes
uint8_t headCount
4.3.5.2.2 Member Data Documentation
The documentation for this struct was generated from the following files:
source/
source/
channel
enum CAN_RX_FIFO_CHANNELS channel
headCount
uint8_t headCount
4.3.5.3 CAN_MSG_FIELD Struct Reference
Used to configure the message fields of CAN frame.
4.3.5.3.1 Detailed Description
Used to configure the message fields of CAN frame.
#include <can_types.h>
Public Attributes
uint8_t idType:1
uint8_t frameType:1
uint8_t dlc:4
uint8_t formatType:1
uint8_t brs:1
4.3.5.3.2 Member Data Documentation
brs
uint8_t brs
Enables or Disables the Bit Rate Switch (width:1 bit)
dlc
uint8_t dlc
Defines the size of the data bytes in a message frame. The maximum DLC is 8 for CAN 2.0 and 64 for CAN FD (width: 4 bit)
formatType
uint8_t formatType
Defines the message type as CAN 2.0 Format or CAN_FD Format (width: 1 bit)
frameType
uint8_t frameType
Defines the message frame type as Data Frame or RTR Frame (1 bit)
idType
uint8_t idType
Defines the message ID type as Standard ID or Extended ID (width: 1 bit)
4.3.5.4 CAN_MSG_OBJ Struct Reference
Used to configure the message object of CAN frame.
4.3.5.4.1 Detailed Description
Used to configure the message object of CAN frame.
#include <can_types.h>
Public Attributes
uint32_t msgId
struct CAN_MSG_FIELD field
uint8_t * data
4.3.5.4.2 Member Data Documentation
data
uint8_t* data
Pointer to message data
field
struct CAN_MSG_FIELD field
For CAN TX/RX Message Object Control
msgId
uint32_t msgId
Set the CAN Message ID (EID <17:0> | SID <10:0>)
4.3.6 File Documentation
4.3.6.1 source/can1_interrupt.c File Reference
#include <string.h> #include "../can1.h"
4.3.6.1.1 Data structures
struct CAN1_FIFOREG
Defines a structure to access CAN1 FIFO Registers.
struct CAN1_RX_FIFO_MSG
CAN1 Receive FIFO Message Object head count information maintenance data structure.
4.3.6.1.2 Functions
static uint8_t CAN1_DlcToDataBytesGet (const enum CAN_DLC dlc)
Get the DLC enum based data byte value.
static uint8_t CAN1_PLSIZEToPayloadBytesGet (uint8_t plsize)
Get the Payload size in bytes for PLSIZE register value.
static bool CAN1_IsTxChannel (uint8_t channel)
Check if a valid channel is configured as transmitter or not.
static enum CAN_TX_FIFO_STATUS CAN1_GetTxFifoStatus (uint8_t validChannel)
Returns the CAN1 transmit FIFO status.
static void CAN1_MessageWriteToFifo (uint8_t *txFifoObj, struct CAN_MSG_OBJ *txCanMsg)
Reads the message object from user input and updates the CAN1 TX FIFO.
static enum CAN_TX_MSG_REQUEST_STATUS CAN1_ValidateTransmission (uint8_t channel, struct CAN_MSG_OBJ *txCanMsg)
Validates transmission.
static void CAN1_RX_FIFO_ResetInfo (void)
Resets the CAN1 receive message head count.
static bool CAN1_IsRxChannel (uint8_t channel)
Checks if a valid channel is configured as receiver or not.
static uint8_t CAN1_GetRxFifoStatus (uint8_t validChannel)
Returns the CAN1 Receive FIFO status.
static uint8_t CAN1_GetRxFifoDepth (uint8_t validChannel)
Returns the CAN1 Receive FIFO depth.
static void CAN1_MessageReadFromFifo (uint8_t *rxFifoObj, struct CAN_MSG_OBJ *rxCanMsg)
Reads the message object from Receive FIFO and updates the user message object.
static bool CAN1_ReceiveFromFiFo (uint8_t index, enum CAN_RX_FIFO_CHANNELS channel, struct CAN_MSG_OBJ *rxCanMsg)
Reads the data object from a particular CAN receive FIFO.
static void CAN1_TX_FIFO_Configuration (void)
Configures the CAN1 TX FIFO settings.
static void CAN1_RX_FIFO_Configuration (void)
Configures the CAN1 Receive FIFO settings.
static void CAN1_RX_FIFO_FilterMaskConfiguration (void)
Configures the CAN1 RX FIFO filter and mask settings.
static void CAN1_BitRateConfiguration (void)
Configures the CAN1 Bit rate settings.
static void CAN1_ErrorNotificationEnable (void)
Enables the CAN1 error notification interrupt.
void CAN1_Initialize (void)
Initializes the CAN1 module.
void CAN1_Deinitialize (void)
Resets the CAN1 registers and settings to their POR values.
enum CAN_OP_MODE_STATUS CAN1_OperationModeSet (const enum CAN_OP_MODES requestMode)
Sets the CAN1 Operation mode.
enum CAN_OP_MODES CAN1_OperationModeGet (void)
Gets the CAN1 Operation mode.
enum CAN_TX_MSG_REQUEST_STATUS CAN1_Transmit (const enum CAN_TX_FIFO_CHANNELS fifoChannel, struct CAN_MSG_OBJ *txCanMsg)
Writes the CAN message object to the specified transmit FIFO channel.
enum CAN_TX_FIFO_STATUS CAN1_TransmitFIFOStatusGet (const enum CAN_TX_FIFO_CHANNELS fifoChannel)
Returns the CAN1 transmitter FIFO status.
bool CAN1_IsTxErrorPassive (void)
Returns the Transmit Error Passive state. If the Transmit Error Counter is above 127, then the transmitter is in Error Passive state.
bool CAN1_IsTxErrorWarning (void)
Returns the Transmit Error Warning state. If the Transmit Error Counter is above 95 and below 128, then the transmitter is in Error Warning state.
bool CAN1_IsTxErrorActive (void)
Returns the Transmit Error Active state. If the Transmit Error Counter is above 0 and below 128, then the transmitter is in Error Active state.
bool CAN1_Receive (struct CAN_MSG_OBJ *rxCanMsg)
Reads a message object.
bool CAN1_ReceiveMessageGet (const enum CAN_RX_FIFO_CHANNELS fifoChannel, struct CAN_MSG_OBJ *rxCanMsg)
Reads a message object from the selected CAN1 receive FIFO.
uint8_t CAN1_ReceivedMessageCountGet (void)
Returns the number of CAN messages received in all the FIFOs.
uint8_t CAN1_ReceiveFIFOStatusGet (const enum CAN_RX_FIFO_CHANNELS fifoChannel)
Returns the CAN1 receiver FIFO status.
bool CAN1_IsRxErrorPassive (void)
Returns the Receive Error Passive state. If the Receive Error Counter is above 127, then the receiver is in Error Passive state.
bool CAN1_IsRxErrorWarning (void)
Returns the Receive Error Warning state. If the Receive Error Counter is above 95 and below 128, then the receiver is in Error Warning state.
bool CAN1_IsRxErrorActive (void)
Returns the Receive Error Active state. If the Receive Error Counter is above 0 and below 128, then the receiver is in Error Active state.
bool CAN1_IsBusOff (void)
Returns the Bus Off status.
void CAN1_Sleep (void)
Puts the CAN1 node into Sleep mode.
void CAN1_InvalidMessageCallbackRegister (void(*handler)(void))
Setter function for the CAN1_InvalidMessage callback.
void CAN1_BusWakeUpActivityCallbackRegister (void(*handler)(void))
Setter function for the CAN1_BusWakeUpActivity callback.
void CAN1_BusErrorCallbackRegister (void(*handler)(void))
Setter function for the CAN1_BusError callback.
void CAN1_ModeChangeCallbackRegister (void(*handler)(void))
Setter function for the CAN1_ModeChange callback.
void CAN1_SystemErrorCallbackRegister (void(*handler)(void))
Setter function for the CAN1_SystemError callback.
void CAN1_TxAttemptCallbackRegister (void(*handler)(void))
Setter function for the CAN1_TxAttempt callback.
void CAN1_RxBufferOverFlowCallbackRegister (void(*handler)(void))
Setter function for the CAN1_RxBufferOverFlow callback.
void CAN1_TXQEmptyCallbackRegister (void(*handler)(void))
Setter function for the CAN1_TXQEmpty callback.
void CAN1_FIFO1HalfEmptyCallbackRegister (void(*handler)(void))
Setter function for the CAN1_FIFO1HalfEmpty callback.
void CAN1_FIFO2NotEmptyCallbackRegister (void(*handler)(void))
Setter function for the CAN1_FIFO2NotEmpty callback.
void CAN1_FIFO3FullCallbackRegister (void(*handler)(void))
Setter function for the CAN1_FIFO3Full callback.
-
If vectored interrupt is used:
void __interrupt (irq(CAN), base(8))
void __interrupt (irq(CANTX), base(8))
void __interrupt (irq(CANRX), base(8))
-
If legacy interrupt is used:
void CAN1_InformationISR(void)
void CAN1_TransmitISR(void)
void CAN1_ReceiveISR(void)
4.3.6.1.3 Macros
CAN Bus Receive FIFO Memory information
Macros for the CAN Bus Receive FIFO Memory.
#define CAN1_NUM_OF_RX_FIFO (2U)
#define CAN1_RX_FIFO_MSG_DATA (64U)
4.3.6.1.4 CAN1 Message object arbitration and control field information
Macros for the CAN1 Message object arbitration and control field.
4.3.6.1.5 Variables
const struct CAN_INTERFACE CAN_FD1
Structure object of type CAN_INTERFACE with the custom name given by the user.
static void(* CAN1_InvalidMessageHandler )(void) = NULL
static void(* CAN1_BusWakeUpActivityHandler )(void) = NULL
static void(* CAN1_BusErrorHandler )(void) = NULL
static void(* CAN1_ModeChangeHandler )(void) = NULL
static void(* CAN1_SystemErrorHandler )(void) = NULL
static void(* CAN1_TxAttemptHandler )(void) = NULL
static void(* CAN1_RxBufferOverFlowHandler )(void) = NULL
static void(* CAN1_TXQEmptyHandler )(void) = NULL
static void(* CAN1_FIFO1HalfEmptyHandler )(void) = NULL
static void(* CAN1_FIFO2NotEmptyHandler )(void) = NULL
static void(* CAN1_FIFO3FullHandler )(void) = NULL
static uint8_t rxMsgData [CAN1_RX_FIFO_MSG_DATA]
static volatile struct CAN1_RX_FIFO_MSG rxFIFOMsg [CAN1_NUM_OF_RX_FIFO]
static volatile struct CAN1_FIFOREG *const FIFO = (struct CAN1_FIFOREG *)&C1TXQCONL
4.3.6.1.6 Function Documentation
__interrupt(irq(CAN))
void __interrupt (irq(CAN) , base(8) )
__interrupt(irq(CANRX))
void __interrupt (irq(CANRX) , base(8) )
__interrupt(irq(CANTX))
void __interrupt (irq(CANTX) , base(8) )
4.3.6.1.7 Macro Definition Documentation
CAN1_NUM_OF_RX_FIFO
#define CAN1_NUM_OF_RX_FIFO (2U)
CAN1_RX_FIFO_MSG_DATA
#define CAN1_RX_FIFO_MSG_DATA (64U)
CAN_MSG_OBJ_BRS_FIELD_MASK
#define CAN_MSG_OBJ_BRS_FIELD_MASK (0x40U)
CAN_MSG_OBJ_BRS_POSN
#define CAN_MSG_OBJ_BRS_POSN (0x6U)
CAN_MSG_OBJ_DLC_FIELD_MASK
#define CAN_MSG_OBJ_DLC_FIELD_MASK (0xFU)
CAN_MSG_OBJ_EID_HIGH_MASK
#define CAN_MSG_OBJ_EID_HIGH_MASK (0x1FU)
CAN_MSG_OBJ_EID_HIGH_WIDTH
#define CAN_MSG_OBJ_EID_HIGH_WIDTH (0x5U)
CAN_MSG_OBJ_EID_LOW_MASK
#define CAN_MSG_OBJ_EID_LOW_MASK (0xF8U)
CAN_MSG_OBJ_EID_LOW_POSN
#define CAN_MSG_OBJ_EID_LOW_POSN (0x3U)
CAN_MSG_OBJ_EID_LOW_WIDTH
#define CAN_MSG_OBJ_EID_LOW_WIDTH (0x5U)
CAN_MSG_OBJ_EID_MID_MASK
#define CAN_MSG_OBJ_EID_MID_MASK (0xFFU)
CAN_MSG_OBJ_EID_MID_WIDTH
#define CAN_MSG_OBJ_EID_MID_WIDTH (0x8U)
CAN_MSG_OBJ_FDF_FIELD_MASK
#define CAN_MSG_OBJ_FDF_FIELD_MASK (0x80U)
CAN_MSG_OBJ_FDF_POSN
#define CAN_MSG_OBJ_FDF_POSN (0x7U)
CAN_MSG_OBJ_FRAME_TYPE_FIELD_MASK
#define CAN_MSG_OBJ_FRAME_TYPE_FIELD_MASK (0x20U)
CAN_MSG_OBJ_ID_TYPE_FIELD_MASK
#define CAN_MSG_OBJ_ID_TYPE_FIELD_MASK (0x10U)
CAN_MSG_OBJ_IDE_POSN
#define CAN_MSG_OBJ_IDE_POSN (0x4U)
CAN_MSG_OBJ_RTR_POSN
#define CAN_MSG_OBJ_RTR_POSN (0x5U)
CAN_MSG_OBJ_SID_HIGH_MASK
#define CAN_MSG_OBJ_SID_HIGH_MASK (0x7U)
CAN_MSG_OBJ_SID_HIGH_WIDTH
#define CAN_MSG_OBJ_SID_HIGH_WIDTH (0x3U)
CAN_MSG_OBJ_SID_LOW_MASK
#define CAN_MSG_OBJ_SID_LOW_MASK (0xFFU)
CAN_MSG_OBJ_SID_LOW_WIDTH
#define CAN_MSG_OBJ_SID_LOW_WIDTH (0x8U)
CAN_STD_MSG_ID_SIZE
#define CAN_STD_MSG_ID_SIZE (CAN_MSG_OBJ_SID_LOW_WIDTH + CAN_MSG_OBJ_SID_HIGH_WIDTH)
4.3.6.1.8 Variable Documentation
CAN1_BusErrorHandler
void(* CAN1_BusErrorHandler) (void) = NULL[static]
CAN1_BusWakeUpActivityHandler
void(* CAN1_BusWakeUpActivityHandler) (void) = NULL[static]
CAN1_FIFO1HalfEmptyHandler
void(* CAN1_FIFO1HalfEmptyHandler) (void) = NULL[static]
CAN1_FIFO2NotEmptyHandler
void(* CAN1_FIFO2NotEmptyHandler) (void) = NULL[static]
CAN1_FIFO3FullHandler
void(* CAN1_FIFO3FullHandler) (void) = NULL[static]
CAN1_InvalidMessageHandler
void(* CAN1_InvalidMessageHandler) (void) = NULL[static]
CAN1_ModeChangeHandler
void(* CAN1_ModeChangeHandler) (void) = NULL[static]
CAN1_RxBufferOverFlowHandler
void(* CAN1_RxBufferOverFlowHandler) (void) = NULL[static]
CAN1_SystemErrorHandler
void(* CAN1_SystemErrorHandler) (void) = NULL[static]
CAN1_TxAttemptHandler
void(* CAN1_TxAttemptHandler) (void) = NULL[static]
CAN1_TXQEmptyHandler
void(* CAN1_TXQEmptyHandler) (void) = NULL[static]
FIFO
volatile struct CAN1_FIFOREG* const FIFO = (struct CAN1_FIFOREG *)&C1TXQCONL[static]
rxFIFOMsg
volatile struct CAN1_RX_FIFO_MSG rxFIFOMsg[CAN1_NUM_OF_RX_FIFO][static]
Initial value:
= { {CAN1_FIFO_2, 0U}, {CAN1_FIFO_3, 0U}, }
rxMsgData
uint8_t rxMsgData[CAN1_RX_FIFO_MSG_DATA][static]
4.3.6.2 source/can1_interrupt.h File Reference
#include <xc.h> #include <stdbool.h> #include <stdint.h> #include "can_types.h" #include "can_interface.h"
4.3.6.2.1 Functions
void CAN1_Initialize (void)
Initializes the CAN1 module.
void CAN1_Deinitialize (void)
Resets the CAN1 registers and settings to their POR values.
enum CAN_OP_MODE_STATUS CAN1_OperationModeSet (const enum CAN_OP_MODES requestMode)
Sets the CAN1 Operation mode.
enum CAN_OP_MODES CAN1_OperationModeGet (void)
Gets the CAN1 Operation mode.
enum CAN_TX_MSG_REQUEST_STATUS CAN1_Transmit (const enum CAN_TX_FIFO_CHANNELS fifoChannel, struct CAN_MSG_OBJ *txCanMsg)
Writes the CAN message object to the specified transmit FIFO channel.
enum CAN_TX_FIFO_STATUS CAN1_TransmitFIFOStatusGet (const enum CAN_TX_FIFO_CHANNELS fifoChannel)
Returns the CAN1 transmitter FIFO status.
bool CAN1_IsTxErrorPassive (void)
Returns the Transmit Error Passive state. If the Transmit Error Counter is above 127, then the transmitter is in Error Passive state.
bool CAN1_IsTxErrorWarning (void)
Returns the Transmit Error Warning state. If the Transmit Error Counter is above 95 and below 128, then the transmitter is in Error Warning state.
bool CAN1_IsTxErrorActive (void)
Returns the Transmit Error Active state. If the Transmit Error Counter is above 0 and below 128, then the transmitter is in Error Active state.
bool CAN1_Receive (struct CAN_MSG_OBJ *rxCanMsg)
Reads a message object.
bool CAN1_ReceiveMessageGet (const enum CAN_RX_FIFO_CHANNELS fifoChannel, struct CAN_MSG_OBJ *rxCanMsg)
Reads a message object from the selected CAN1 receive FIFO.
uint8_t CAN1_ReceivedMessageCountGet (void)
Returns the number of CAN messages received in all the FIFOs.
uint8_t CAN1_ReceiveFIFOStatusGet (const enum CAN_RX_FIFO_CHANNELS fifoChannel)
Returns the CAN1 receiver FIFO status.
bool CAN1_IsRxErrorPassive (void)
Returns the Receive Error Passive state. If the Receive Error Counter is above 127, then the receiver is in Error Passive state.
bool CAN1_IsRxErrorWarning (void)
Returns the Receive Error Warning state. If the Receive Error Counter is above 95 and below 128, then the receiver is in Error Warning state.
bool CAN1_IsRxErrorActive (void)
Returns the Receive Error Active state. If the Receive Error Counter is above 0 and below 128, then the receiver is in Error Active state.
bool CAN1_IsBusOff (void)
Returns the Bus Off status.
void CAN1_Sleep (void)
Puts the CAN1 node into Sleep mode.
void CAN1_InvalidMessageCallbackRegister (void(*handler)(void))
Setter function for the CAN1_InvalidMessage callback.
void CAN1_BusWakeUpActivityCallbackRegister (void(*handler)(void))
Setter function for the CAN1_BusWakeUpActivity callback.
void CAN1_BusErrorCallbackRegister (void(*handler)(void))
Setter function for the CAN1_BusError callback.
void CAN1_ModeChangeCallbackRegister (void(*handler)(void))
Setter function for the CAN1_ModeChange callback.
void CAN1_SystemErrorCallbackRegister (void(*handler)(void))
Setter function for the CAN1_SystemError callback.
void CAN1_TxAttemptCallbackRegister (void(*handler)(void))
Setter function for the CAN1_TxAttempt callback.
void CAN1_RxBufferOverFlowCallbackRegister (void(*handler)(void))
Setter function for the CAN1_RxBufferOverFlow callback.
void CAN1_TXQEmptyCallbackRegister (void(*handler)(void))
Setter function for the CAN1_TXQEmpty callback.
void CAN1_FIFO1HalfEmptyCallbackRegister (void(*handler)(void))
Setter function for the CAN1_FIFO1HalfEmpty callback.
void CAN1_FIFO2NotEmptyCallbackRegister (void(*handler)(void))
Setter function for the CAN1_FIFO2NotEmpty callback.
void CAN1_FIFO3FullCallbackRegister (void(*handler)(void))
Setter function for the CAN1_FIFO3Full callback.
4.3.6.2.2 Macros
#define CAN_FD1_Initialize CAN1_Initialize
Defines the Custom Name for CAN1_Initialize() API.
#define CAN_FD1_Deinitialize CAN1_Deinitialize
Defines the Custom Name for CAN1_Deinitialize() API.
#define CAN_FD1_OperationModeSet CAN1_OperationModeSet
Defines the Custom Name for CAN1_OperationModeSet() API.
#define CAN_FD1_OperationModeGet CAN1_OperationModeGet
Defines the Custom Name for CAN1_OperationModeGet() API.
#define CAN_FD1_Transmit CAN1_Transmit
Defines the Custom Name for CAN1_Transmit() API.
#define CAN_FD1_TransmitFIFOStatusGet CAN1_TransmitFIFOStatusGet
Defines the Custom Name for CAN1_TransmitFIFOStatusGet() API.
#define CAN_FD1_IsTxErrorPassive CAN1_IsTxErrorPassive
Defines the Custom Name for CAN1_IsTxErrorPassive() API.
#define CAN_FD1_IsTxErrorWarning CAN1_IsTxErrorWarning
Defines the Custom Name for CAN1_IsTxErrorWarning() API.
#define CAN_FD1_IsTxErrorActive CAN1_IsTxErrorActive
Defines the Custom Name for CAN1_IsTxErrorActive() API.
#define CAN_FD1_Receive CAN1_Receive
Defines the Custom Name for CAN1_Receive() API.
#define CAN_FD1_ReceiveMessageGet CAN1_ReceiveMessageGet
Defines the Custom Name for CAN1_ReceiveMessageGet() API.
#define CAN_FD1_ReceivedMessageCountGet CAN1_ReceivedMessageCountGet
Defines the Custom Name for CAN1_ReceivedMessageCountGet() API.
#define CAN_FD1_ReceiveFIFOStatusGet CAN1_ReceiveFIFOStatusGet
Defines the Custom Name for CAN1_ReceiveFIFOStatusGet() API.
#define CAN_FD1_IsRxErrorPassive CAN1_IsRxErrorPassive
Defines the Custom Name for CAN1_IsRxErrorPassive() API.
#define CAN_FD1_IsRxErrorWarning CAN1_IsRxErrorWarning
Defines the Custom Name for CAN1_IsRxErrorWarning() API.
#define CAN_FD1_IsRxErrorActive CAN1_IsRxErrorActive
Defines the Custom Name for CAN1_IsRxErrorActive() API.
#define CAN_FD1_IsBusOff CAN1_IsBusOff
Defines the Custom Name for CAN1_IsBusOff() API.
#define CAN_FD1_Sleep CAN1_Sleep
Defines the Custom Name for CAN1_Sleep() API.
#define CAN_FD1_InvalidMessageCallbackRegister CAN1_InvalidMessageCallbackRegister
Defines the Custom Name for CAN1_InvalidMessageCallbackRegister() API.
#define CAN_FD1_BusWakeUpActivityCallbackRegister CAN1_BusWakeUpActivityCallbackRegister
Defines the Custom Name for CAN1_BusWakeUpActivityCallbackRegister() API.
#define CAN_FD1_BusErrorCallbackRegister CAN1_BusErrorCallbackRegister
Defines the Custom Name for CAN1_BusErrorCallbackRegister() API.
#define CAN_FD1_ModeChangeCallbackRegister CAN1_ModeChangeCallbackRegister
Defines the Custom Name for CAN1_ModeChangeCallbackRegister() API.
#define CAN_FD1_SystemErrorCallbackRegister CAN1_SystemErrorCallbackRegister
Defines the Custom Name for CAN1_SystemErrorCallbackRegister() API.
#define CAN_FD1_TxAttemptCallbackRegister CAN1_TxAttemptCallbackRegister
Defines the Custom Name for CAN1_TxAttemptCallbackRegister() API.
#define CAN_FD1_RxBufferOverFlowCallbackRegister CAN1_RxBufferOverFlowCallbackRegister
Defines the Custom Name for CAN1_RxBufferOverFlowCallbackRegister() API.
#define CAN1_TX_TXQ CAN1_TXQ
CAN1 Transmit FIFO TXQ Custom Name.
#define CAN1_TX_FIFO1 CAN1_FIFO_1
CAN1 Transmit FIFO 1 Custom Name.
#define CAN1_RX_FIFO2 CAN1_FIFO_2
CAN1 Receive FIFO 2 Custom Name.
#define CAN1_RX_FIFO3 CAN1_FIFO_3
CAN1 Receive FIFO 3 Custom Name.
4.3.6.2.3 Variables
const struct CAN_INTERFACE CAN_FD1
Structure object of type CAN_INTERFACE with the custom name given by the user.
4.3.6.3 source/can1_polling.c File Reference
#include <string.h> #include "../can1.h"
4.3.6.3.1 Data structures
struct CAN1_FIFOREG
Defines a structure to access CAN1 FIFO Registers.
struct CAN1_RX_FIFO_MSG
CAN1 Receive FIFO Message Object head count information maintenance data structure.
4.3.6.3.2 Functions
static uint8_t CAN1_DlcToDataBytesGet (const enum CAN_DLC dlc)
Get the DLC enum based data byte value.
static uint8_t CAN1_PLSIZEToPayloadBytesGet (uint8_t plsize)
Get the Payload size in bytes for PLSIZE register value.
static bool CAN1_IsTxChannel (uint8_t channel)
Check if a valid channel is configured as transmitter or not.
static enum CAN_TX_FIFO_STATUS CAN1_GetTxFifoStatus (uint8_t validChannel)
Returns the CAN1 transmit FIFO status.
static void CAN1_MessageWriteToFifo (uint8_t *txFifoObj, struct CAN_MSG_OBJ *txCanMsg)
Reads the message object from user input and updates the CAN1 TX FIFO.
static enum CAN_TX_MSG_REQUEST_STATUS CAN1_ValidateTransmission (uint8_t channel, struct CAN_MSG_OBJ *txCanMsg)
Validates transmission.
static void CAN1_RX_FIFO_ResetInfo (void)
Resets the CAN1 receive message head count.
static bool CAN1_IsRxChannel (uint8_t channel)
Checks if a valid channel is configured as receiver or not.
static uint8_t CAN1_GetRxFifoStatus (uint8_t validChannel)
Returns the CAN1 Receive FIFO status.
static uint8_t CAN1_GetRxFifoDepth (uint8_t validChannel)
Returns the CAN1 Receive FIFO depth.
static void CAN1_MessageReadFromFifo (uint8_t *rxFifoObj, struct CAN_MSG_OBJ *rxCanMsg)
Reads the message object from Receive FIFO and updates the user message object.
static bool CAN1_ReceiveFromFiFo (uint8_t index, enum CAN_RX_FIFO_CHANNELS channel, struct CAN_MSG_OBJ *rxCanMsg)
Reads the data object from a particular CAN receive FIFO.
static void CAN1_TX_FIFO_Configuration (void)
Configures the CAN1 TX FIFO settings.
static void CAN1_RX_FIFO_Configuration (void)
Configures the CAN1 Receive FIFO settings.
static void CAN1_RX_FIFO_FilterMaskConfiguration (void)
Configures the CAN1 RX FIFO filter and mask settings.
static void CAN1_BitRateConfiguration (void)
Configures the CAN1 Bit rate settings.
void CAN1_Initialize (void)
Initializes the CAN1 module.
void CAN1_Deinitialize (void)
Resets the CAN1 registers and settings to their POR values.
enum CAN_OP_MODE_STATUS CAN1_OperationModeSet (const enum CAN_OP_MODES requestMode)
Sets the CAN1 Operation mode.
enum CAN_OP_MODES CAN1_OperationModeGet (void)
Gets the CAN1 Operation mode.
enum CAN_TX_MSG_REQUEST_STATUS CAN1_Transmit (const enum CAN_TX_FIFO_CHANNELS fifoChannel, struct CAN_MSG_OBJ *txCanMsg)
Writes the CAN message object to the specified transmit FIFO channel.
enum CAN_TX_FIFO_STATUS CAN1_TransmitFIFOStatusGet (const enum CAN_TX_FIFO_CHANNELS fifoChannel)
Returns the CAN1 transmitter FIFO status.
bool CAN1_IsTxErrorPassive (void)
Returns the Transmit Error Passive state. If the Transmit Error Counter is above 127, then the transmitter is in Error Passive state.
bool CAN1_IsTxErrorWarning (void)
Returns the Transmit Error Warning state. If the Transmit Error Counter is above 95 and below 128, then the transmitter is in Error Warning state.
bool CAN1_IsTxErrorActive (void)
Returns the Transmit Error Active state. If the Transmit Error Counter is above 0 and below 128, then the transmitter is in Error Active state.
bool CAN1_Receive (struct CAN_MSG_OBJ *rxCanMsg)
Reads a message object.
bool CAN1_ReceiveMessageGet (const enum CAN_RX_FIFO_CHANNELS fifoChannel, struct CAN_MSG_OBJ *rxCanMsg)
Reads a message object from the selected CAN1 receive FIFO.
uint8_t CAN1_ReceivedMessageCountGet (void)
Returns the number of CAN messages received in all the FIFOs.
uint8_t CAN1_ReceiveFIFOStatusGet (const enum CAN_RX_FIFO_CHANNELS fifoChannel)
Returns the CAN1 receiver FIFO status.
bool CAN1_IsRxErrorPassive (void)
Returns the Receive Error Passive state. If the Receive Error Counter is above 127, then the receiver is in Error Passive state.
bool CAN1_IsRxErrorWarning (void)
Returns the Receive Error Warning state. If the Receive Error Counter is above 95 and below 128, then the receiver is in Error Warning state.
bool CAN1_IsRxErrorActive (void)
Returns the Receive Error Active state. If the Receive Error Counter is above 0 and below 128, then the receiver is in Error Active state.
bool CAN1_IsBusOff (void)
Returns the Bus Off status.
void CAN1_Sleep (void)
Puts the CAN1 node into Sleep mode.
void CAN1_InvalidMessageCallbackRegister (void(*handler)(void))
Setter function for the CAN1_InvalidMessage callback.
void CAN1_BusWakeUpActivityCallbackRegister (void(*handler)(void))
Setter function for the CAN1_BusWakeUpActivity callback.
void CAN1_BusErrorCallbackRegister (void(*handler)(void))
Setter function for the CAN1_BusError callback.
void CAN1_ModeChangeCallbackRegister (void(*handler)(void))
Setter function for the CAN1_ModeChange callback.
void CAN1_SystemErrorCallbackRegister (void(*handler)(void))
Setter function for the CAN1_SystemError callback.
void CAN1_TxAttemptCallbackRegister (void(*handler)(void))
Setter function for the CAN1_TxAttempt callback.
void CAN1_RxBufferOverFlowCallbackRegister (void(*handler)(void))
Setter function for the CAN1_RxBufferOverFlow callback.
void __interrupt (irq(CAN), base(8))
void CAN1_Tasks (void)
Used to implement the tasks for polled implementations.
4.3.6.3.3 Macros
CAN Bus Receive FIFO Memory information
Macros for the CAN Bus Receive FIFO Memory.
#define CAN1_NUM_OF_RX_FIFO (2U)
#define CAN1_RX_FIFO_MSG_DATA (64U)
4.3.6.3.4 CAN1 Message object arbitration and control field information
Macros for the CAN1 Message object arbitration and control field.
4.3.6.3.5 Variables
const struct CAN_INTERFACE CAN_FD1
Structure object of type CAN_INTERFACE with the custom name given by the user.
static void(* CAN1_InvalidMessageHandler )(void) = NULL
static void(* CAN1_BusWakeUpActivityHandler )(void) = NULL
static void(* CAN1_BusErrorHandler )(void) = NULL
static void(* CAN1_ModeChangeHandler )(void) = NULL
static void(* CAN1_SystemErrorHandler )(void) = NULL
static void(* CAN1_TxAttemptHandler )(void) = NULL
static void(* CAN1_RxBufferOverFlowHandler )(void) = NULL
static uint8_t rxMsgData [CAN1_RX_FIFO_MSG_DATA]
static volatile struct CAN1_RX_FIFO_MSG rxFIFOMsg [CAN1_NUM_OF_RX_FIFO]
static volatile struct CAN1_FIFOREG *const FIFO = (struct CAN1_FIFOREG *)&C1TXQCONL
4.3.6.3.6 Function Documentation
__interrupt()
void __interrupt (irq(CAN) , base(8) )
CAN1_BitRateConfiguration()
static void CAN1_BitRateConfiguration (void )[static]
Configures the CAN1 Bit rate settings.
None. |
None. |
CAN1_DlcToDataBytesGet()
static uint8_t CAN1_DlcToDataBytesGet (const enum CAN_DLC dlc)[static]
Get the DLC enum based data byte value.
in | dlc |
- DLC value as described in CAN_DLC. |
The data byte value coresponding to DLC. |
CAN1_GetRxFifoDepth()
static uint8_t CAN1_GetRxFifoDepth (uint8_t validChannel)[static]
Returns the CAN1 Receive FIFO depth.
in | validChannel |
- Receive FIFO channel as described in CAN_RX_FIFO_CHANNELS. |
Depth of the Receive FIFO. |
CAN1_GetRxFifoStatus()
static uint8_t CAN1_GetRxFifoStatus (uint8_t validChannel)[static]
Returns the CAN1 Receive FIFO status.
in | validChannel |
- Receive FIFO channel as described in CAN_RX_FIFO_CHANNELS. |
Status of the CAN1 Receive FIFO. Refer CAN_RX_FIFO_STATUS for details. |
CAN1_GetTxFifoStatus()
static enum CAN_TX_FIFO_STATUS CAN1_GetTxFifoStatus (uint8_t validChannel)[static]
Returns the CAN1 transmit FIFO status.
in | channel |
- Transmit FIFO channel as described in CAN_TX_FIFO_CHANNELS. |
Status of the CAN1 Transmit FIFO as described in CAN_TX_FIFO_STATUS. |
CAN1_IsRxChannel()
static bool CAN1_IsRxChannel (uint8_t channel)[static]
Checks if a valid channel is configured as receiver or not.
in | channel |
- Receive FIFO channel as described in CAN_RX_FIFO_CHANNELS. |
True |
- FIFO channel is configured as receiver. |
False |
- FIFO channel is not configured as receiver. |
CAN1_IsTxChannel()
static bool CAN1_IsTxChannel (uint8_t channel)[static]
Check if a valid channel is configured as transmitter or not.
in | channel |
- Transmit FIFO channel as described in CAN_TX_FIFO_CHANNELS. |
True |
- FIFO channel is configured as transmitter. |
False |
- FIFO channel is not configured as transmitter. |
CAN1_MessageReadFromFifo()
static void CAN1_MessageReadFromFifo (uint8_t * rxFifoObj, struct CAN_MSG_OBJ * rxCanMsg)[static]
Reads the message object from Receive FIFO and updates the user message object.
in | rxFifoObj |
- Receive FIFO message object. |
out | rxCanMsg |
- Pointer to the message object of type CAN_MSG_OBJ. |
None. |
CAN1_MessageWriteToFifo()
static void CAN1_MessageWriteToFifo (uint8_t * txFifoObj, struct CAN_MSG_OBJ * txCanMsg)[static]
Reads the message object from user input and updates the CAN1 TX FIFO.
out | txFifoObj |
- Transmit FIFO message object. |
in | txCanMsg |
- Pointer to the message object of type CAN_MSG_OBJ. |
None. |
CAN1_PLSIZEToPayloadBytesGet()
static uint8_t CAN1_PLSIZEToPayloadBytesGet (uint8_t plsize)[static]
Get the Payload size in bytes for PLSIZE register value.
in | plsize |
- The value in PLSIZE register. |
The number of data bytes corresponding to PLSIZE register value. |
CAN1_ReceiveFromFiFo()
static bool CAN1_ReceiveFromFiFo (uint8_t index, enum CAN_RX_FIFO_CHANNELS channel, struct CAN_MSG_OBJ * rxCanMsg)[static]
Reads the data object from a particular CAN receive FIFO.
in | index |
- Instance of Receive FIFO. |
in | channel |
- Receive FIFO channel as described in CAN_RX_FIFO_CHANNELS. |
out | rxCanMsg |
- Pointer to the message object of type CAN_MSG_OBJ. |
True |
- CAN1 message read succeeded. |
False |
- CAN1 message read failed. |
CAN1_RX_FIFO_Configuration()
static void CAN1_RX_FIFO_Configuration (void )[static]
Configures the CAN1 Receive FIFO settings.
None. |
None. |
CAN1_RX_FIFO_FilterMaskConfiguration()
static void CAN1_RX_FIFO_FilterMaskConfiguration (void )[static]
Configures the CAN1 RX FIFO filter and mask settings.
None. |
None. |
CAN1_RX_FIFO_ResetInfo()
static void CAN1_RX_FIFO_ResetInfo (void )[static]
Resets the CAN1 receive message head count.
None. |
None. |
CAN1_TX_FIFO_Configuration()
static void CAN1_TX_FIFO_Configuration (void )[static]
Configures the CAN1 TX FIFO settings.
None. |
None. |
CAN1_ValidateTransmission()
static enum CAN_TX_MSG_REQUEST_STATUS CAN1_ValidateTransmission (uint8_t channel, struct CAN_MSG_OBJ * txCanMsg)[static]
Validates transmission.
in | channel |
- Transmit FIFO channel as described in CAN_TX_FIFO_CHANNELS. |
in | txCanMsg |
- Pointer to the message object of type CAN_MSG_OBJ. |
Status of the CAN1 Transmit operation as described in CAN_TX_MSG_REQUEST_STATUS. |
4.3.6.3.7 Macro Definition Documentation
CAN1_NUM_OF_RX_FIFO
#define CAN1_NUM_OF_RX_FIFO (2U)
CAN1_RX_FIFO_MSG_DATA
#define CAN1_RX_FIFO_MSG_DATA (64U)
CAN_MSG_OBJ_BRS_FIELD_MASK
#define CAN_MSG_OBJ_BRS_FIELD_MASK (0x40U)
CAN_MSG_OBJ_BRS_POSN
#define CAN_MSG_OBJ_BRS_POSN (0x6U)
CAN_MSG_OBJ_DLC_FIELD_MASK
#define CAN_MSG_OBJ_DLC_FIELD_MASK (0xFU)
CAN_MSG_OBJ_EID_HIGH_MASK
#define CAN_MSG_OBJ_EID_HIGH_MASK (0x1FU)
CAN_MSG_OBJ_EID_HIGH_WIDTH
#define CAN_MSG_OBJ_EID_HIGH_WIDTH (0x5U)
CAN_MSG_OBJ_EID_LOW_MASK
#define CAN_MSG_OBJ_EID_LOW_MASK (0xF8U)
CAN_MSG_OBJ_EID_LOW_POSN
#define CAN_MSG_OBJ_EID_LOW_POSN (0x3U)
CAN_MSG_OBJ_EID_LOW_WIDTH
#define CAN_MSG_OBJ_EID_LOW_WIDTH (0x5U)
CAN_MSG_OBJ_EID_MID_MASK
#define CAN_MSG_OBJ_EID_MID_MASK (0xFFU)
CAN_MSG_OBJ_EID_MID_WIDTH
#define CAN_MSG_OBJ_EID_MID_WIDTH (0x8U)
CAN_MSG_OBJ_FDF_FIELD_MASK
#define CAN_MSG_OBJ_FDF_FIELD_MASK (0x80U)
CAN_MSG_OBJ_FDF_POSN
#define CAN_MSG_OBJ_FDF_POSN (0x7U)
CAN_MSG_OBJ_FRAME_TYPE_FIELD_MASK
#define CAN_MSG_OBJ_FRAME_TYPE_FIELD_MASK (0x20U)
CAN_MSG_OBJ_ID_TYPE_FIELD_MASK
#define CAN_MSG_OBJ_ID_TYPE_FIELD_MASK (0x10U)
CAN_MSG_OBJ_IDE_POSN
#define CAN_MSG_OBJ_IDE_POSN (0x4U)
CAN_MSG_OBJ_RTR_POSN
#define CAN_MSG_OBJ_RTR_POSN (0x5U)
CAN_MSG_OBJ_SID_HIGH_MASK
#define CAN_MSG_OBJ_SID_HIGH_MASK (0x7U)
CAN_MSG_OBJ_SID_HIGH_WIDTH
#define CAN_MSG_OBJ_SID_HIGH_WIDTH (0x3U)
CAN_MSG_OBJ_SID_LOW_MASK
#define CAN_MSG_OBJ_SID_LOW_MASK (0xFFU)
CAN_MSG_OBJ_SID_LOW_WIDTH
#define CAN_MSG_OBJ_SID_LOW_WIDTH (0x8U)
CAN_STD_MSG_ID_SIZE
#define CAN_STD_MSG_ID_SIZE (CAN_MSG_OBJ_SID_LOW_WIDTH + CAN_MSG_OBJ_SID_HIGH_WIDTH)
4.3.6.3.8 Variable Documentation
CAN1_BusErrorHandler
void(* CAN1_BusErrorHandler) (void) = NULL[static]
CAN1_BusWakeUpActivityHandler
void(* CAN1_BusWakeUpActivityHandler) (void) = NULL[static]
CAN1_InvalidMessageHandler
void(* CAN1_InvalidMessageHandler) (void) = NULL[static]
CAN1_ModeChangeHandler
void(* CAN1_ModeChangeHandler) (void) = NULL[static]
CAN1_RxBufferOverFlowHandler
void(* CAN1_RxBufferOverFlowHandler) (void) = NULL[static]
CAN1_SystemErrorHandler
void(* CAN1_SystemErrorHandler) (void) = NULL[static]
CAN1_TxAttemptHandler
void(* CAN1_TxAttemptHandler) (void) = NULL[static]
FIFO
volatile struct CAN1_FIFOREG* const FIFO = (struct CAN1_FIFOREG *)&C1TXQCONL[static]
rxFIFOMsg
volatile struct CAN1_RX_FIFO_MSG rxFIFOMsg[CAN1_NUM_OF_RX_FIFO][static]
Initial value:
= { {CAN1_FIFO_2, 0U}, {CAN1_FIFO_3, 0U}, }
rxMsgData
uint8_t rxMsgData[CAN1_RX_FIFO_MSG_DATA][static]
4.3.6.4 source/can1_polling.h File Reference
#include <xc.h> #include <stdbool.h> #include <stdint.h> #include "can_types.h" #include "can_interface.h"
4.3.6.4.1 Functions
void CAN1_Initialize (void)
Initializes the CAN1 module.
void CAN1_Deinitialize (void)
Resets the CAN1 registers and settings to their POR values.
enum CAN_OP_MODE_STATUS CAN1_OperationModeSet (const enum CAN_OP_MODES requestMode)
Sets the CAN1 Operation mode.
enum CAN_OP_MODES CAN1_OperationModeGet (void)
Gets the CAN1 Operation mode.
enum CAN_TX_MSG_REQUEST_STATUS CAN1_Transmit (const enum CAN_TX_FIFO_CHANNELS fifoChannel, struct CAN_MSG_OBJ *txCanMsg)
Writes the CAN message object to the specified transmit FIFO channel.
enum CAN_TX_FIFO_STATUS CAN1_TransmitFIFOStatusGet (const enum CAN_TX_FIFO_CHANNELS fifoChannel)
Returns the CAN1 transmitter FIFO status.
bool CAN1_IsTxErrorPassive (void)
Returns the Transmit Error Passive state. If the Transmit Error Counter is above 127, then the transmitter is in Error Passive state.
bool CAN1_IsTxErrorWarning (void)
Returns the Transmit Error Warning state. If the Transmit Error Counter is above 95 and below 128, then the transmitter is in Error Warning state.
bool CAN1_IsTxErrorActive (void)
Returns the Transmit Error Active state. If the Transmit Error Counter is above 0 and below 128, then the transmitter is in Error Active state.
bool CAN1_Receive (struct CAN_MSG_OBJ *rxCanMsg)
Reads a message object.
bool CAN1_ReceiveMessageGet (const enum CAN_RX_FIFO_CHANNELS fifoChannel, struct CAN_MSG_OBJ *rxCanMsg)
Reads a message object from the selected CAN1 receive FIFO.
uint8_t CAN1_ReceivedMessageCountGet (void)
Returns the number of CAN messages received in all the FIFOs.
uint8_t CAN1_ReceiveFIFOStatusGet (const enum CAN_RX_FIFO_CHANNELS fifoChannel)
Returns the CAN1 receiver FIFO status.
bool CAN1_IsRxErrorPassive (void)
Returns the Receive Error Passive state. If the Receive Error Counter is above 127, then the receiver is in Error Passive state.
bool CAN1_IsRxErrorWarning (void)
Returns the Receive Error Warning state. If the Receive Error Counter is above 95 and below 128, then the receiver is in Error Warning state.
bool CAN1_IsRxErrorActive (void)
Returns the Receive Error Active state. If the Receive Error Counter is above 0 and below 128, then the receiver is in Error Active state.
bool CAN1_IsBusOff (void)
Returns the Bus Off status.
void CAN1_Sleep (void)
Puts the CAN1 node into Sleep mode.
void CAN1_InvalidMessageCallbackRegister (void(*handler)(void))
Setter function for the CAN1_InvalidMessage callback.
void CAN1_BusWakeUpActivityCallbackRegister (void(*handler)(void))
Setter function for the CAN1_BusWakeUpActivity callback.
void CAN1_BusErrorCallbackRegister (void(*handler)(void))
Setter function for the CAN1_BusError callback.
void CAN1_ModeChangeCallbackRegister (void(*handler)(void))
Setter function for the CAN1_ModeChange callback.
void CAN1_SystemErrorCallbackRegister (void(*handler)(void))
Setter function for the CAN1_SystemError callback.
void CAN1_TxAttemptCallbackRegister (void(*handler)(void))
Setter function for the CAN1_TxAttempt callback.
void CAN1_RxBufferOverFlowCallbackRegister (void(*handler)(void))
Setter function for the CAN1_RxBufferOverFlow callback.
void CAN1_Tasks (void)
Used to implement the tasks for polled implementations.
4.3.6.4.2 Macros
#define CAN_FD1_Initialize CAN1_Initialize
Defines the Custom Name for CAN1_Initialize() API.
#define CAN_FD1_Deinitialize CAN1_Deinitialize
Defines the Custom Name for CAN1_Deinitialize() API.
#define CAN_FD1_OperationModeSet CAN1_OperationModeSet
Defines the Custom Name for CAN1_OperationModeSet() API.
#define CAN_FD1_OperationModeGet CAN1_OperationModeGet
Defines the Custom Name for CAN1_OperationModeGet() API.
#define CAN_FD1_Transmit CAN1_Transmit
Defines the Custom Name for CAN1_Transmit() API.
#define CAN_FD1_TransmitFIFOStatusGet CAN1_TransmitFIFOStatusGet
Defines the Custom Name for CAN1_TransmitFIFOStatusGet() API.
#define CAN_FD1_IsTxErrorPassive CAN1_IsTxErrorPassive
Defines the Custom Name for CAN1_IsTxErrorPassive() API.
#define CAN_FD1_IsTxErrorWarning CAN1_IsTxErrorWarning
Defines the Custom Name for CAN1_IsTxErrorWarning() API.
#define CAN_FD1_IsTxErrorActive CAN1_IsTxErrorActive
Defines the Custom Name for CAN1_IsTxErrorActive() API.
#define CAN_FD1_Receive CAN1_Receive
Defines the Custom Name for CAN1_Receive() API.
#define CAN_FD1_ReceiveMessageGet CAN1_ReceiveMessageGet
Defines the Custom Name for CAN1_ReceiveMessageGet() API.
#define CAN_FD1_ReceivedMessageCountGet CAN1_ReceivedMessageCountGet
Defines the Custom Name for CAN1_ReceivedMessageCountGet() API.
#define CAN_FD1_ReceiveFIFOStatusGet CAN1_ReceiveFIFOStatusGet
Defines the Custom Name for CAN1_ReceiveFIFOStatusGet() API.
#define CAN_FD1_IsRxErrorPassive CAN1_IsRxErrorPassive
Defines the Custom Name for CAN1_IsRxErrorPassive() API.
#define CAN_FD1_IsRxErrorWarning CAN1_IsRxErrorWarning
Defines the Custom Name for CAN1_IsRxErrorWarning() API.
#define CAN_FD1_IsRxErrorActive CAN1_IsRxErrorActive
Defines the Custom Name for CAN1_IsRxErrorActive() API.
#define CAN_FD1_IsBusOff CAN1_IsBusOff
Defines the Custom Name for CAN1_IsBusOff() API.
#define CAN_FD1_Sleep CAN1_Sleep
Defines the Custom Name for CAN1_Sleep() API.
#define CAN_FD1_InvalidMessageCallbackRegister CAN1_InvalidMessageCallbackRegister
Defines the Custom Name for CAN1_InvalidMessageCallbackRegister() API.
#define CAN_FD1_BusWakeUpActivityCallbackRegister CAN1_BusWakeUpActivityCallbackRegister
Defines the Custom Name for CAN1_BusWakeUpActivityCallbackRegister() API.
#define CAN_FD1_BusErrorCallbackRegister CAN1_BusErrorCallbackRegister
Defines the Custom Name for CAN1_BusErrorCallbackRegister() API.
#define CAN_FD1_ModeChangeCallbackRegister CAN1_ModeChangeCallbackRegister
Defines the Custom Name for CAN1_ModeChangeCallbackRegister() API.
#define CAN_FD1_SystemErrorCallbackRegister CAN1_SystemErrorCallbackRegister
Defines the Custom Name for CAN1_SystemErrorCallbackRegister() API.
#define CAN_FD1_TxAttemptCallbackRegister CAN1_TxAttemptCallbackRegister
Defines the Custom Name for CAN1_TxAttemptCallbackRegister() API.
#define CAN_FD1_RxBufferOverFlowCallbackRegister CAN1_RxBufferOverFlowCallbackRegister
Defines the Custom Name for CAN1_RxBufferOverFlowCallbackRegister() API.
#define CAN1_TX_TXQ CAN1_TXQ
CAN1 Transmit FIFO TXQ Custom Name.
#define CAN1_TX_FIFO1 CAN1_FIFO_1
CAN1 Transmit FIFO 1 Custom Name.
#define CAN1_RX_FIFO2 CAN1_FIFO_2
CAN1 Receive FIFO 2 Custom Name.
#define CAN1_RX_FIFO3 CAN1_FIFO_3
CAN1 Receive FIFO 3 Custom Name.
#define CAN_FD1_Tasks CAN1_Tasks
Defines the Custom Name for CAN1_Tasks() API.
4.3.6.4.3 Variables
const struct CAN_INTERFACE CAN_FD1
Structure object of type CAN_INTERFACE with the custom name given by the user.
4.3.6.5 source/can_features.h File Reference
This is the generated module feature header file for CAN driver. This file provides module feature list available on the selected device.
4.3.6.5.1 Macros
#define CAN_FD_MESSAGE_FORMAT_FEATURE_AVAILABLE 1
Defines the CAN FD Message format data update request functionality.
#define CAN_FIFO_BASED_TRANSMIT_PRIORITY_FEATURE_AVAILABLE 1
Defines the CAN FIFO based transmit priority data update request functionality.
#define CAN_DMA_INTERFACE_FEATURE_AVAILABLE 0
Defines the CAN 2.0 DMA interface data update request functionality.
4.3.6.5.2 Detailed Description
This is the generated module feature header file for CAN driver. This file provides module feature list available on the selected device.
CAN Generated Feature Header File
The macros defined in this file provides the flexibility to easily migrate the user application to other device which might have varied feature list.
The file has to be manually included in main.c, if the user intends to migrate the application to another device which might have varied feature list.
The content in this file is strictly "read only" and should not be altered. Failing to do so, the migration is not guaranteed.
CAN Driver Version 1.0.0 |
4.3.6.6 source/can_types.h File Reference
This is the generated driver types header file for the CAN driver.
#include <stdint.h>
4.3.6.6.1 Data structures
struct CAN_MSG_FIELD
Used to configure the message fields of CAN frame.
struct CAN_MSG_OBJ
Used to configure the message object of CAN frame.
4.3.6.6.2 Enumerations
enum CAN_TX_FIFO_CHANNELS { CAN1_TXQ = 0, CAN1_FIFO_1 = 1, CAN_TX_FIFO_MAX }
Defines the CAN FIFOs configured as transmit.
enum CAN_RX_FIFO_CHANNELS { CAN1_FIFO_2 = 2, CAN1_FIFO_3 = 3, CAN_RX_FIFO_MAX }
Defines the CAN FIFOs configured as receive.
enum CAN_MSG_OBJ_BRS_MODE { CAN_NON_BRS_MODE = 0, CAN_BRS_MODE = 1 }
Defines if the bit rate switching is enabled or disabled in the CAN message object.
enum CAN_MSG_OBJ_ID_TYPE { CAN_FRAME_STD = 0, CAN_FRAME_EXT = 1 }
Defines if the message ID is Standard ID or Extended ID in CAN message object.
enum CAN_MSG_OBJ_FRAME_TYPE { CAN_FRAME_DATA = 0, CAN_FRAME_RTR = 1 }
Defines if the frame type is Data frame or Remote Transmit Request frame in CAN message object.
enum CAN_MSG_OBJ_TYPE { CAN_2_0_FORMAT = 0, CAN_FD_FORMAT = 1 }
Defines if the CAN message object is in CAN FD format or CAN 2.0 format.
enum CAN_TX_MSG_REQUEST_STATUS { CAN_TX_MSG_REQUEST_SUCCESS = 0, CAN_TX_MSG_REQUEST_DLC_EXCEED_ERROR = 1, CAN_TX_MSG_REQUEST_BRS_ERROR = 2, CAN_TX_MSG_REQUEST_FIFO_FULL = 3 }
Defines the CAN transmit API return status.
enum CAN_OP_MODES { CAN_NORMAL_FD_MODE = 0x0, CAN_DISABLE_MODE = 0x1, CAN_INTERNAL_LOOPBACK_MODE = 0x2, CAN_LISTEN_ONLY_MODE = 0x3, CAN_CONFIGURATION_MODE = 0x4, CAN_EXTERNAL_LOOPBACK_MODE = 0x5, CAN_NORMAL_2_0_MODE = 0x6, CAN_RESTRICTED_OPERATION_MODE =0x7 }
Defines the CAN operation modes that are available for the module to use.
enum CAN_OP_MODE_STATUS { CAN_OP_MODE_REQUEST_SUCCESS, CAN_OP_MODE_REQUEST_FAIL, CAN_OP_MODE_SYS_ERROR_OCCURED }
Defines the return status of CAN operation mode set API.
enum CAN_TX_FIFO_STATUS { CAN_TX_FIFO_FULL = 0x0, CAN_TX_FIFO_AVAILABLE = 0x1 }
Defines the status of CAN FD transmit FIFO.
enum CAN_RX_FIFO_STATUS { CAN_RX_MSG_NOT_AVAILABLE = 0x0, CAN_RX_MSG_AVAILABLE = 0x1, CAN_RX_MSG_OVERFLOW = 0x8 }
Defines the CAN FD receive FIFO status bit mask values.
enum CAN_DLC { DLC_0, DLC_1, DLC_2, DLC_3, DLC_4, DLC_5, DLC_6, DLC_7, DLC_8, DLC_12, DLC_16, DLC_20, DLC_24, DLC_32, DLC_48, DLC_64 }
Defines the CAN message payload sizes that are available for the mode to use.
4.3.6.6.3 Detailed Description
This is the generated driver types header file for the CAN driver.
CAN Generated Driver Types Header File