2.2.1.4 I/O Protection Key
The Verify, ECDH, , and
KDF commands can optionally use the I/O protection feature to
encrypt some parameters and validate (via MAC) some responses. This is to help protect
against man-in-the-middle attacks on the physical I2C bus. However, before
this feature can be used, the MCU and ATECC608A-TNGTLS need
to generate and save a unique I/O protection key, essentially pairing the MCU and ATECC608A-TNGTLS devices to each other. The pairing process
must happen on first boot.
I/O Protection Key Generation:
- MCU uses random command to generate a random 32-byte I/O protection key.
- MCU saves the I/O protection key in its internal Flash.
- MCU writes I/O protection key to the I/O protection key slot.
- MCU slot locks that slot to make the I/O protection key permanent.
As a pairing check, the MCU could use the MAC command to
issue a challenge to the I/O protection key and verify the I/O protection key stored in
Flash matches the one in the ATECC608A-TNGTLS.