5.3.3.4 GenDig - Shared Nonce
In Shared Nonce mode 32 bytes of data are input to this command. This mode is used
when a nonce value must be shared between two devices. The Nonce
command must be run prior to the first GenDig command to load a value
into TempKey. Subsequent GenDig commands will use the value from the
previous GenDig operation.
|
Opcode |
Mode |
KeyID(1) |
Data | Description |
|---|---|---|---|---|
| 0x15 | 0x03 | 0x00 0[Slot] | Input data | |
| 0x80 0[Slot] | Input data |
Note:
- KeyId specifies the DataZone slot to be used in the TempKey calculation. Only the lowest 32 bytes will be used.
| Name | Size | Description |
|---|---|---|
| Response | 1 byte |
0x00 - If successful. Error code - If the command fails. |
Note:
Flag Bits
- TempKey.Valid flag will be set to 1 if successful, otherwise it is 0.
- TempKey.GenDigData will be set to 1 indicating a DataZone slot was used in the calculation.
- TempKey.KeyID will set to the slot specified in the command.
| Size | Parameters - KeyID MSB 0x00 | Parameters - KeyID MSB 0x80 |
|---|---|---|
| 32 bytes | Input Data | TempKey.value |
| 1 byte | Opcode = 0x15 | Opcode = 0x15 |
| 1 byte | Mode = 0x03 | Mode = 0x03 |
| 1 byte | LSB of KeyID = 0x0[Slot] | LSB of KeyID = 0x0[Slot] |
| 1 byte | 0x00 | 0x00 |
| 1 byte | SN[8] = 0x01 | SN[8] = 0x01 |
| 2 bytes | SN[0:1] = 0x01 0x23 | SN[0:1] = 0x01 0x23 |
| 25 bytes | All Zeros | All Zeros |
| 32 bytes | TempKey.Value | Input Data |