Various GND Bounce Parameters
(Ask a Question)- VOLP (peak) and VOLV (valley) for ground bounce
- VOHP (peak) and VOHV (valley) for VCC bounce
The pulse width parameter or the settling time of the bounce is the time for which the signals stay over a given threshold criterion. As the waveform of a ground bounce pulse looks more like a sinusoid than a square wave, the pulse width depends on the point of measurement. This parameter is important because every input buffer has a limit on the smallest pulse that it can recognize with regard to width and amplitude. A smaller pulse is not recognized, even though the amplitude might be much higher, as shown in the following figure. For example, an input buffer with a minimum recognizable pulse width of 3 ns at 2V does not recognize a pulse that is 1 ns wide, even if its amplitude is 2.5V.
Therefore, with regard to noise, pulse width, and voltage amplitude of the glitch must be minimized so that it is not interpreted as a logic pulse by the input buffer of the receiving device.