1.3.19.2 PORT_PinWrite Function
C
void PORT_PinWrite(PORT_PIN pin, bool value)
Summary
Writes the specified value to the selected pin.
Description
This function writes/drives the "value" on the selected I/O line/pin.
Precondition
The PORT_Initialize() function should have been called once.
Parameters
Param | Description |
---|---|
pin | One of the IO pins from the enum PORT_PIN. |
value | value to be written on the selected pin. - true = set pin to high (1). - false = clear pin to low (0). |
Returns
None.
Example
bool value = true; PORT_PinWrite(PORT_PIN_PB03, value);
Remarks
Calling this function with an input pin with the pull-up/pull-down feature enabled will affect the pull-up/pull-down configuration. If the value is false, the pull-down will be enabled. If the value is true, the pull-up will be enabled.