1.3.19.5 PORT_PinToggle Function
C
void PORT_PinToggle(PORT_PIN pin)
Summary
Toggles the selected pin.
Description
This function toggles/inverts the present value on the selected I/O line/pin.
Precondition
The PORT_Initialize() function should have been called.
Parameters
Param | Description |
---|---|
pin | One of the IO pins from the enum PORT_PIN. |
Returns
None.
Example
PORT_PinToggle(PORT_PIN_PB03);
Remarks
None.