1.39.1.8 ADCx_ConversionSequenceIsFinished Function
C
bool ADCx_ConversionSequenceIsFinished( void ) // x is instance of the peripheral and it is applicable only for devices having multiple instances of the peripheral.
Summary
Returns the status of automatic sequence conversion.
Description
This function checks the status of the conversion sequence.
Precondition
ADC_Initialize() function must have been called first for the associated instance.And conversion must have been started.
Parameters
None.
Returns
True - All the enabled channels in the sequence have finished conversion False - Sequence conversion is ongoing
Example
bool seq_status; ADC0_Initialize(); ADC0_ConversionStart(); seq_status = ADC0_ConversionSequenceIsFinished();
Remarks
This function is valid only if auto sequence feature is enabled.