1.29.18.20 PORT_GROUP Enum
C
The Port Groups vary based on device family. Refer to the generated header file for the actual values.
Summary
Identifies the port groups available on the device.
Description
This enumeration identifies the port groups available on the device.
Remarks
The caller should not use the constant expressions assigned to any of the enumeration constants as these may vary between devices. Port group shown here are representative only. Not all ports groups are available on all devices. Refer to the specific device data sheet to determine which ports are supported. The MHC will generate this enumeration with the port groups that are available on the device.