1.21.14 (PMP)
The Parallel Master Port (PMP) is a parallel 8-bit/16-bit I/O module specifically designed to communicate with a wide variety of parallel devices such as communications peripherals, LCDs, external memory devices and micro-controllers. Because the interfaces to parallel peripherals vary significantly, the PMP module is highly configurable.
Using The Library
The key features of PMP :-
-
8-bit,16-bit interface
-
Up to 16 programmable address lines
-
Up to two Chip Select lines
-
Programmable strobe options
-
Address auto-increment/auto-decrement
-
Programmable address/data multiplexing
-
Programmable polarity on control signals
-
Programmable Wait states
Library Interface
peripheral library provides the following interfaces:
Functions
Name | Description |
---|---|
PMP_Initialize | This function initializes the PMP controller of the device |
PMP_AddressSet | Sets the current address of the PMP module to the specified address |
PMP_AddressGet | Gets the current address of the PMP module |
PMP_MasterSend | Sends the specified data in Master mode |
PMP_MasterReceive | Receives the data in Master mode |
PMP_PortIsBusy | Identifies if the (Master mode) PMP port is busy |
PMP_AddressPortEnable | Enables the port lines specified as PMP address lines |
PMP_AddressPortDisable | Disables the port lines specified as PMP address lines |