1.32.29.7 TCx_Timer16bitPeriodGet Function

C

/* x = TC instance number */
uint16_t TCx_Timer16bitPeriodGet( void );

Summary

Reads the period value of given timer.

Description

This function reads the value of period.

Precondition

TCx_TimerInitialize() function must have been called first.

Parameters

None.

Returns

The timer's period value.

Example

uint16_t period = 0;
TC0_TimerInitialize();
period = TC0_Timer16bitPeriodGet();

Remarks

The caller must know the number of significant bytes of timer. Period value is right-aligned.