1.32.13.5 FREQM_FrequencyGet Function
C
uint32_t FREQM_FrequencyGet(void)
Summary
Returns the measured frequency in Hz.
Description
This function returns the measured frequency in Hz. It should be called when a frequency measurement is complete and no errors have occurred. This function is non-blocking. In this mode, the function should be called only after a callback function was called. The return value of the function is only valid if the FREQM_ErrorGet() function returns FREQM_ERROR_NONE.
Precondition
FREQM_Initialize() and FREQM_MeasurementStart() functions should be called.
Parameters
None.
Returns
Returns frequency value of the measured clock. The value is only valid if the FREQM_ErrorGet() function returns FREQM_ERROR_NONE.
Example
// Refer to the code example of FREQM_CallbackRegister() function for guidance on interrupt based operation. // The following code snippet shows an exampl of non-interrupt based operation. FREQM_Initialize(); FREQM_MeasurementStart() // Wait till the measurement is complete. while(FREQM_IsBusy()); if(FREQM_ERROR_NONE == FREQM_ErrorGet()) { measuredFrequency = FREQM_FrequencyGet(); // This means there are no errors and the value contained in // measuredFrequency is valid. }
Remarks
None.