1.4.20.11 RTC_Timer32CounterGet Function
C
uint32_t RTC_Timer32CounterGet ( void )
Summary
Get the current 32-bit counter value.
Description
This function returns the current 32-bit count value. This function can be used to retrieve the counter value at the end of a time measurement.
Precondition
RTC_Initialize must have been called for the associated RTC instance. The RTC peripheral should have been configured in 32-bit Timer Counter mode
Parameters
None.
Returns
uint32_t returns the current 32 bit counter value.
Example
// The following code example stops the counter when the counter value // has reached 0xFFF. RTC_Initialize(); RTC_Timer32CompareSet(0); RTC_Timer32CounterSet(0); RTC_Timer32Start(); while(RTC_Timer32CounterGet() < 0xFFF); // Stop the counter. RTC_Timer32Stop();
Remarks
None.