1.4.25.16 TCCx_TimerCallbackRegister Function
C
void TCCx_TimerCallbackRegister( TCC_CALLBACK callback, uintptr_t context );
Summary
Registers the function to be called from interrupt.
Description
This function registers the callback function to be called from interrupt.
Precondition
TCCx_TimerInitialize() must have been called first.
Parameters
Param | Description |
---|---|
callback | callback function pointer |
context | Allows the caller to provide a context value (usually a pointer to the callers context for multi-instance clients). |
Returns
None.
Example
void TCC_Callback_Fn( uint32_t status, uintptr_t context );
TCCx_TimerInitialize();
TCCx_TimerCallbackRegister(TCC_Callback_Fn, NULL);
Remarks
Context value can be set to NULL if not required. To disable callback function, pass NULL for the callback parameter.