1.2.24.25 TCCx_Compare16bitMatchSet Function

C

/* x = TCC instance number */
void TCCx_Compare16bitMatchSet( TCCx_CHANNEL_NUM channel, uint16_t compareValue );

Summary

Writes compare value of the given compare channel.

Description

Set compare value of given channel

Precondition

TCCx_CompareInitialize() function must have been called first.

Parameters

Param Description
compareValue value to set for compare channel 0

Returns

None.

Example

uint16_t compareValue = 0x100;
TCC0_CompareInitialize();
TCC0_Compare16bitMatch0Set(TCC0_CHANNEL0, compareValue);

Remarks

None