1.9.22.9 SYSTICK_TimerPeriodHasExpired Function
C
bool SYSTICK_TimerPeriodHasExpired( void )
Summary
Returns the current status of the systick
Description
This function is used to identify if the Systick underflow has happened.
This API is generated only in polling mode
Precondition
SYSTICK_Initialize should have been called to set up SysTick.
Parameters
None.
Returns
True - timer period has expired
False - timer period is not expired
Example
SYSTICK_Initialize(); SYSTICK_TimerStart(); if(SYSTICK_TimerPeriodHasExpired()) { //application code }