1.36.18.8 TCx_CHy_TimerCompareSet Function
C
/* x = TC instance number, y= channel number */ /* 16 bit timer */ void TCx_CHy_TimerCompareSet ( uint16_t compare ); /* 32 bit timer */ void TCx_CHy_TimerCompareSet ( uint32_t compare );
Summary
Sets the compare value of a given timer channel.
Description
This function writes the compare value. When timer counter matches compare value, interrupt can be generated.
Precondition
TCx_CHy_TimerInitialize function must have been called first for the given channel.
Parameters
Param | Description |
---|---|
compare | compare value of the timer (type is based on the bit width of timer) |
Returns
None.
Example
TC0_CH1_TimerInitialize();
TC0_CH1_TimerCompareSet(0x500U);
Remarks
This function is available only when TC timer mode is used by SYS_TIME module. SYS_TIME uses compare match interrupt to generate dynamic delay.