1.33.16.72 SERCOMx_I2C_CommandSet Function
C
/* x = SERCOM instance number */
/* I2C slave mode */
void SERCOMx_I2C_CommandSet(SERCOM_I2C_SLAVE_COMMAND command)
Summary
Sets I2C slave command
Description
Sets I2C slave command. The I2C slave state machine takes action based on the set command.
Precondition
SERCOMx_I2C_Initialize must have been called for the associated SERCOM I2C instance
Parameters
Param | Description |
---|---|
SERCOM_I2C_SLAVE_COMMAND_SEND_ACK | Send ACK succeeded by reception of next byte |
SERCOM_I2C_SLAVE_COMMAND_SEND_NAK | Send NAK succeeded by reception of next byte |
SERCOM_I2C_SLAVE_COMMAND_RECEIVE_ACK_NAK | Execute a byte read operation followed by ACK/NACK reception |
SERCOM_I2C_SLAVE_COMMAND_WAIT_FOR_START | Wait for any start (S/Sr) condition |
Returns
None.
Example
The below code snippet shows how SERCOMx_I2C_CommandSet() API can be used when SERCOM I2C slave PLIB is used in polled mode (interrupt is disabled).
static bool isFirstByteSent; static bool transferDir; // Define a flag that inidicates if the I2C slave application is busy or ready static bool isAppBusy; SERCOM_I2C_SLAVE_INTFLAG intFlags = SERCOM5_I2C_InterruptFlagsGet(); if (intFlags & SERCOM_I2C_SLAVE_INTFLAG_AMATCH) { isFirstByteSent = false; // Read and save the transfer direction in a global variable. transferDir = SERCOM5_I2C_TransferDirGet(); if (isAppBusy == true) { // I2C slave application is busy. Send NAK. SERCOM0_I2C_SendCommand(SERCOM_I2C_SLAVE_COMMAND_SEND_NAK); } else { // I2C slave application is ready. Send ACK succeeded by reception of next byte SERCOM0_I2C_SendCommand(SERCOM_I2C_SLAVE_COMMAND_SEND_ACK); } } else if (intFlags & SERCOM_I2C_SLAVE_INTFLAG_DRDY) { if (transferDir == SERCOM_I2C_SLAVE_TRANSFER_DIR_WRITE) { // I2C master is writing data to I2C slave. Read the received byte. rxByte = SERCOM0_I2C_ReadByte(); // Execute acknowledge action succeeded by reception of next byte SERCOM0_I2C_SendCommand(SERCOM_I2C_SLAVE_COMMAND_SEND_ACK); } else { // I2C master is reading data from I2C slave. Check if the previous data // is acknowledged by the I2C master. if (isFirstByteSent == false) { SERCOM0_I2C_WriteByte(txData); isFirstByteSent = true; } else { if (SERCOM0_I2C_LastByteAckStatusGet() == SERCOM_I2C_SLAVE_ACK_STATUS_RECEIVED_ACK) { // Last byte was acknowledged by the I2C master; send another byte. SERCOM0_I2C_WriteByte(txData); //Execute a byte read operation followed by ACK/NACK reception SERCOM0_I2C_SendCommand(SERCOM_I2C_SLAVE_COMMAND_RECEIVE_ACK_NAK); } else { // Last byte was NAK'd by the I2C master; wait for start condition. //Wait for any start (S/Sr) condition SERCOM0_I2C_SendCommand(SERCOM_I2C_SLAVE_COMMAND_WAIT_FOR_START); } } } } else if (intFlags & SERCOM_I2C_SLAVE_INTFLAG_PREC) { SERCOM0_I2C_InterruptFlagsClear(SERCOM_I2C_SLAVE_INTFLAG_PREC); }
Remarks
This API is generated when Smart mode is disabled and is typically used when the SERCOM I2C slave PLIB is used in polled mode (interrupt is disabled).