1.5.21.44 RTC_TIMER16_CALLBACK Typedef
C
typedef void (*RTC_TIMER16_CALLBACK)( RTC_TIMER16_INT_MASK interruptCause, uintptr_t context );
Summary
Defines the data type and function signature of the RTC 16-bit Timer Counter callback function.
Description
This data type defines the function signature of the RTC 16-bit Timer Counter Callback function. The RTC peripheral will call back the client's function with this signature everytime when the 16-bit Time Counter related event has occurred. Refer to the description of the RTC_TIMER16_INT_MASK enumeration for possible events. Hardware event flags are cleared when the callback function exits.
The application should register a callback function whose signature (input arguments and return type) must match the signature of this function. The callback function should be registered by calling the RTC_Timer16CallbackRegister() function. The callback function should be registered before starting the timer.
Precondition
The RTC_Initialize() function should have been called to initialize the RTC peripheral. The RTC_Timer16CallbackRegister() function should have been called to register the callback function. The RTC peripheral should have been configured for 16-bit Timer Counter mode in MHC. The RTC peripheral should have been configured for Interrupt mode operation in MHC.
Parameters
Param | Description |
---|---|
event | The 16-bit Timer Counter event that caused the callback function to be called. Multiple events can be active. The application should check for all events in the callback function |
context | Allows the caller to provide a context value (usually a pointer to the callers context for multi-instance clients) |
Returns
None.
Example
void MyTimer16Callback (RTC_TIMER16_INT_MASK_COMPARE0_MATCH interruptCause, uintptr_t context ) { if((interruptCause & RTC_TIMER16_EVENT_PERIOD_MATCH) == RTC_TIMER16_EVENT_PERIOD_MATCH) { // The period has matched. } else if((interruptCause & RTC_TIMER16_EVENT_COMPARE1_MATCH) == RTC_TIMER16_EVENT_COMPARE1_MATCH) { // Compare 1 value has matched. } else if((interruptCause & RTC_TIMER16_EVENT_COMPARE0_MATCH) == RTC_TIMER16_EVENT_COMPARE0_MATCH) { // Compare 0 value has matched. } } // Initialize the RTC Peripheral and register the callback function. // Note how the pointer to the peridoicIntervalHadExpired flag is specified // as the context. This is passed back into the callback function. RTC_Initialize(); RTC_Timer16CounterSet(0); RTC_Timer16PeriodSet(0xFFF); RTC_Timer16CallbackRegister(MyTimer16Callback, NULL); RTC_Timer16Start();
Remarks
This callback if only available when the RTC peripheral is configured for 16-bit Timer Counter operation. The callback function will be execute in an interrupt context. Avoid calling blocking , computationally intensive or interrupt un-safe function from the callback function.