1.14.9.4 EVIC_SourceIsEnabled Function
C
bool EVIC_SourceIsEnabled( INT_SOURCE source )
Summary
Gets the enable state of the interrupt source.
Description
This function gets the enable state of the interrupt source.
Precondition
EVIC_Initialize() function must have been called first.
Parameters
Param | Description |
---|---|
source | One of the possible values from INT_SOURCE. |
Returns
-
true: If the interrupt source is enabled
-
false: If the interrupt source is disabled
Example
if(EVIC_SourceIsEnabled(INT_SOURCE_CORE_TIMER) != true) { EVIC_SourceEnable(INT_SOURCE_CORE_TIMER); }
Remarks
This function implements an operation of the SourceControl feature. This feature may not be available on all devices. Please refer to the specific device data sheet to determine availability.