1.23.15.11 NVM_ProgramFlashWriteProtect Function
C
The prototype of NVM_ProgramFlashWriteProtect() varies based on device family. Refer to the generated header file for the actual prototype to be used.
void NVM_ProgramFlashWriteProtect( uint32_t address ); void NVM_ProgramFlashWriteProtect( uint32_t lt_address, uint32_t gte_address );
Summary
Protect Program Flash Memory from Writes
Description
For NVM_ProgramFlashWriteProtect( uint32_t address )
-
Protects the Program Flash Page in which the address falls and all the lower pages below it from writes. Passing address value as 0 will unlock the entire program flash memory for writes.
For NVM_ProgramFlashWriteProtect( uint32_t lt_address, uint32_t gte_address )
-
Protects the Program pages at Flash addresses less than the "lt_address" and the pages at Flash addresses greater than or equal to "gte_address". Passing address value as 0 will unlock the entire program flash memory for writes.
Precondition
None
Parameters
Param | Description |
---|---|
address | 24-Bit address till where the memory has to be protected from start of flash memory. |
lt_address | Pages at Flash addresses less than this value are write protected |
gte_address | Pages at Flash addresses greater than or equal to this value are write protected. |
Returns
None.
Example
// Protects Memory locations 0x9D000000 - 0x9D001000 NVM_ProgramFlashWriteProtect(0x9D001000);
// Protects Memory locations below 0x9D001000 and Memory locations above 0x9D003000 NVM_ProgramFlashWriteProtect(0x9D001000, 0x9D003000);