1.4.13.12 NVMCTRL_DataScrambleKeySet Function
C
void NVMCTRL_DataScrambleKeySet ( uint32_t dsckey )
Summary
Sets the key for data scrambling of the Secure Data Flash
Description
This function is used to set the key for data scrambling of the Secure Data Flash.
Precondition
Data scrambling has to be disabled using NVMCTRL_DataScrambleEnable() function before calling this function to set the key.
Parameters
Param | Description |
---|---|
dsckey | Data Scramble Key. |
Returns
None.
Example
// Disable Data Scrambling NVMCTRL_DataScrambleEnable(false); NVMCTRL_DataScrambleKeySet(0x123456);
Remarks
This NVMCTRL_DataScrambleKeySet() function is only available in trustZone supported devices.