1.10.16.3 PMP_AddressGet Function
C
uint32_t PMP_AddressGet( void )
Summary
Gets the current address of the PMP module.
Description
This function gets the current address of the PMP module.
Precondition
PMP should have been initialized by calling PMP_Initialize.
Parameters
None.
Returns
address - Device address
Example
uint32_t address; PMP_Initialize(); address = PLIB_PMP_AddressGet();
Remarks
None.