1.36.8.4 MEM2MEM_ChannelCallbackRegister Function
C
void MEM2MEM_ChannelCallbackRegister(MEM2MEM_CALLBACK callback, uintptr_t context)
Summary
This function allows a MEM2MEM PLIB client to set a callback.
Description
This function allows a client to set a callback. The client may want to receive transfer related events in cases when it submits a MEM2MEM PLIB transfer request. The callback should be set before the client intends to perform operations that could generate events.
This function accepts a context parameter. This parameter could be set by the client to contain (or point to) any client specific data object that should be associated with this MEM2MEM channel.
Precondition
None.
Parameters
Param | Description |
---|---|
callback | Pointer to the callback function. |
context | Value identifying the context of the application/driver/middleware that registered the event handling function |
Returns
None.
Example
MY_APP_OBJ myAppObj;
void APP_MEM2MEMTransferEventHandler(MEM2MEM_TRANSFER_EVENT event,
uintptr_t contextHandle)
{
switch(event)
{
case MEM2MEM_TRANSFER_COMPLETE:
// This means the data was transferred.
break;
case MEM2MEM_TRANSFER_ERROR:
// Error handling here.
break;
default:
break;
}
}
// User registers an callback with MEM2MEM channel. This is done once.
MEM2MEM_ChannelCallbackRegister(APP_MEM2MEMTransferEventHandler, (uintptr_t)&myAppObj);
Remarks
None.