1.10.6.2 CORETIMER_CallbackSet Function
C
void CORETIMER_CallbackSet(CORETIMER_CALLBACK callback_fn,
uintptr_t context);
Summary
Sets the callback_fn function for an match.
Description
This function sets the callback_fn function that will be called when the CORETIMER match is reached.
Precondition
CORETIMER_Initialize() function must have been called first.
Parameters
Param | Description |
---|---|
callback_fn | a pointer to the function to be called when match is reached. Use NULL to Un Register the match callback_fn |
context | a pointer to user defined data to be used when the callback_fn function is called. NULL can be passed in if no data needed |
Returns
None.
Example
void CORETIMER_Callback_Fn(uintptr_t context);
CORETIMER_Initialize();
CORETIMER_CallbackSet(CORETIMER_Callback_Fn, NULL);
Remarks
Context value can be set to NULL if not required. To disable callback function, pass NULL for the callback parameter.