1.5.22.56 TCx_CaptureCallbackRegister Function
C
/* x = TC instance number */
void TCx_CaptureCallbackRegister( TC_CAPTURE_CALLBACK callback, uintptr_t context);
Summary
Registers the function to be called from interrupt.
Description
This function registers the callback function to be called from interrupt.
Precondition
TCx_CaptureInitialize() must have been called first.
Parameters
Param | Description |
---|---|
callback | callback function pointer |
context | Allows the caller to provide a context value (usually a pointer to the callers context for multi-instance clients) |
Returns
None.
Example
void TC_Callback_Fn( uintptr_t context );
TC0_CaptureInitialize();
TC0_CaptureCallbackRegister(TC_Callback_Fn, NULL);
Remarks
Context value can be set to NULL if not required. To disable callback function, pass NULL for the callback parameter.