1.19.1.7 ADC_InputScanSelect Function

C

void ADC_InputScanSelect(ADC_INPUTS_SCAN scanInputs);

Summary

Selects input for scanning ADC channels.

Description

This function updates input channels which will be scanned for MUX A. Previous scanning list will be removed, if any.

Precondition

  • ADC_Initialize() must have been called.

  • ADC module should be disabled.

Parameters

Param Description
scanInputs Selects any of the possible positive input from enum ADC_INPUTS_SCAN. User can OR multiple enum elements to select multiple scan channels at one go.

Returns

None.

Example

ADC_InputScanSelect(ADC_INPUT_SCAN_AN2 | ADC_INPUT_SCAN_AN12 | ADC_INPUT_SCAN_AN5);

Remarks

None.