1.32.7.4 DAC_Channel0ResultGet Function

C

uint16_t DAC_Channel0ResultGet (void);

Summary

Returns the Channel 0 Filter output

Description

This function returns the value of the Channel 0 Filter output

Precondition

DAC_Initialize() function must have been called first.

Parameters

None.

Returns

result - Channel 0 Filter output

Example

uint16_t result = 0;
DAC_Initialize ();
result = DAC_Channel0ResultGet ();

Remarks

None.